Click here to return to the Basic DSP page
The RMSWithTC block computes the RMS of the input signals with time constant specified in the text field.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
RMSWithTC | Schematic/Block | Schematic/Block | NA |
Name | Type | Description |
---|---|---|
Input0 | Audio | Input channel 0 |
Name | Type | Description |
---|---|---|
Output0 | Audio | Output channel 0 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
TimeConstant | 121 | 1-1000 | Determines how rapidly the RMS value is to be computed with any change in the input level |
IsDBps | False | True/False | Control value in dB/s or ms |
NumChannels | 2 | 15 | Number of input/Output channels. Change in this value requires re-compilation |
Parameter Name | Description | ADSP-214xx/215xx/SC5xx |
---|---|---|
TimeConstant | TC for RMS value with change in input | Float |
TimeConstant = ABS(1-10^(TimeConstant(linear)/(10*FS))) Where FS is the Sampling rate