Wiki

This version (02 Jan 2023 10:56) was approved by Jagan M.The Previously approved version (21 Jun 2012 20:59) is available.Diff

Click here to return to the Basic DSP section.

Real-Time Display



Description

The Real-Time Display block lets allow us read the data from the target and display it in the graph.

Usage

Click on the “Graph” icon to open the real-time display graph window. 'Start' button allows to read the data from the target for specified time of 'Time Span' and 'Stop' allows us to to stop readback from the target. 'Continous Read' allows us to read the data from the target irrespective of 'Time Span'. 'Reset' resets the graph and Format allows us to specify the format of reading data.

Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
Real Time Display Block/Schematic Block/Schematic Schematic


Pins

Input

NameTypeDescription
Input Audio Input Channel 0

Output

NameTypeDescription
Output Audio Output channel 0


Configurable Parameters

GUI Parameter Default Value Range Function Description
Y-Max/Y-Min1 -134999999 to 134999999 Displays the input signal in the specified y-axis scale
Multiplier11 to 100multiplies the input signal by this value
TimeSpan11 to 20x-axis scale- upper limit on the display

DSP Parameters

Parameter Name Description ADSP-214xx/SC5xx/215xx ADAU145x/146x
ReadDataContains the input signal data Float FixedPoint8d24


resources/tools-software/sigmastudio/toolbox/basicdsp/realtimedisplay.txt · Last modified: 22 Apr 2022 15:52 by Jagan M