This is an old revision of the document!
Click here to return to the Basic DSP page
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Input | any - any | Input signal that is monitored for the first falling edge |
Pin 1: Reset | any - control | Resets the output trigger signal back to zero |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Trigger | any - control | Output flag signal set to “1” in the selected bit position |
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Output Bit Designation | 28 | [28.0 Bit26] | Sets bit position of the output “1” flag. 28.0 is the default values which represents 1LSB. |
GUI Control Name | Compiler Name | Function Description |
---|---|---|
Output Bit Designation | OneShotFallAlg1output1 | Actual value written to DSP from the representation of the drop-down menu to select the bit position of the output “1” flag. |
The following graph shows the output response based on a given input signal and reset signal through the OneShotRiseReset block. In the graphs the input signal is only toggling between “1” and “0” however this algorithm will respond to any changes in level of the input signal, thus the first rising edge of the input signal will trigger the output to go high.
The format of the “1” output value of the is designated by the drop-down menu. The following table shows the “1” Output that corresponds to the drop-down menu selection.
The following image shows the OneShotFallReset block being used with a LFO triangle source, reset switch, and GPIO output. When the LFO is turned on, the output will go high on the first rise of the triangle waveform. The output can be reset when the switch is turned on.
Toolbox Path | Basic DSP - Logic - Toggle - OneShot rise, reset |
Cores Supported | AD1940 ADAU170x ADAU144x ADAU176x ADAU178x |
“Grow Algorithm” Supported | no |
“Add Algorithm” Supported | no |
Subroutine/Loop Based | no |
Program RAM | 9 |
Data RAM | 4 |
Parameter RAM | 1 |