Wiki

This version (24 Jun 2021 09:19) was approved by Sakthivel Perumal.The Previously approved version (19 Dec 2017 10:41) is available.Diff

Click here to return to the Basic DSP page


Block MinMaxLimit (ADAU145x)

MinMaxLimit is a block processing module which compares each input sample in block of input samples with constant values entered text box.

Input Pins

NameFormat [int/dec/float] - [control/audio]Function Description
Pin 0: Input decimal-audio Input signal to the module

Output Pins

NameFormat [int/dec/float] - [control/audio]Function Description
Pin 0: Output decimal-audio Output signal from the module

Grow Algorithm

The module supports growth of input and output channels up to 16 dependently. Add Algorithm is not supported.

GUI Controls

GUI Control NameDefault ValueRangeFunction Description
_MaxLimit 1 -128-127.99Constant value used compare with input samples
_MinLimit 0 -128-127.99Constant value used compare with input samples

DSP Parameter Information

GUI Control NameCompiler NameFunction Description
_MaxLimitMinMaxLimitS300BlkAlg1_MaxLimitConstant value to compare with input samples
_MinLimitMinMaxLimitS300BlkAlg1_MinLimitConstant value to compare with input samples

Here,

  • Green - Algorithm Name
  • Red - Instance Number (Changes for each instance)
  • Blue - Parameter Name

Algorithm Description

This module compares the input samples in an input block of samples with Max Limit and Min Limit values specified in the textbox.

Supported IC's

ADAU145x
ADAU146x
resources/tools-software/sigmastudio/toolbox/basicdsp/minmaxlimit.txt · Last modified: 24 Jun 2021 09:19 by Sakthivel Perumal