This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:basicdsp:externalspidelay [22 Nov 2016 07:17] – Venkatesan Krishnamoorthy | resources:tools-software:sigmastudio:toolbox:basicdsp:externalspidelay [01 Jul 2019 13:15] (current) – Added Growth and multiple instance support Sanjeeva Reddy | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== External SPI Delay (ADAU145X) | + | ====== External SPI Delay ====== |
[[: | [[: | ||
|| | || | ||
Line 21: | Line 21: | ||
\\ | \\ | ||
===== Grow Algorithm ===== | ===== Grow Algorithm ===== | ||
- | The module | + | The module |
\\ | \\ | ||
\\ | \\ | ||
Line 31: | Line 31: | ||
^GUI Control Name^Default Value^Range^Function Description^ | ^GUI Control Name^Default Value^Range^Function Description^ | ||
|Bit Rate|100kHZ| 100 kHZ - 100000 kHZ |SPI Speed| | |Bit Rate|100kHZ| 100 kHZ - 100000 kHZ |SPI Speed| | ||
- | |Default Chip/ Device Address|1| 1-7 |Slave Select for the SPI. Register window should be configured to match this selection.Please refer the note below.| | + | |Default Chip/ Device Address|0| 0-6 |Slave Select for the SPI. Register window should be configured to match this selection.Please refer the note below.| |
|Sub-Address Bytes|2| 1-4 |Number of address bytes excluding the read/write command | | |Sub-Address Bytes|2| 1-4 |Number of address bytes excluding the read/write command | | ||
|Ram Size|128KB|0-32MB|Total Size of RAM used for delay buffer| | |Ram Size|128KB|0-32MB|Total Size of RAM used for delay buffer| | ||
Line 43: | Line 43: | ||
\\ | \\ | ||
\\ | \\ | ||
- | **Note:**If the Default Chip/ Device Address | + | **Note:**If the Slave Select |
{{ : | {{ : | ||
Line 56: | Line 56: | ||
^ ' Default chip/Device Address' | ^ ' Default chip/Device Address' | ||
- | | 2 | + | | 1 |
- | | 4 | + | | 2 |
- | | 16 | + | | 3 |
- | | 32 | + | | 4 |
- | | 64 | + | | 5 |
- | | 128 | + | | 6 |
\\ | \\ | ||
=====DSP Parameter Information===== | =====DSP Parameter Information===== | ||
^GUI Control Name^Compiler Name^Function Description^ | ^GUI Control Name^Compiler Name^Function Description^ | ||
- | |Cur|ADAU145XConfigurableExtRamDelayAlg1delay|Current Delay value in bytes. (Cur * 4)| | + | |Cur|<fc # |
===== Supported ICs ===== | ===== Supported ICs ===== | ||
- ADAU145x | - ADAU145x | ||