This is an old revision of the document!
Click here to return to the Basic DSP section.
This module can be used to implement off-chip delay using the SPI interface.
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Input Data | decimal - control | Value to be updated in the selected parameter |
NA
The module support the algorithm growth up to 16. The input pin will be added for each algorithm instance and user has to select the parameter for all the algorithm instances. If parameter is not selected for any of the instance then the module will not update any parameter.
The selection of the parameter will be enabled only when the schematic compilation is completed successfully. The user can select the module for which the parameter needs to be updated. After selecting the module, the parameter within the module should be selected for which value should be updated. The value of the selected parameter will be updated with the given input value for each sample once the schematic is downloaded. User can also change the parameter selection when the schematic is downloaded. It will start updating the newly selected parameter once the parameter selection window is closed.
The selection window lists the parameters of the modules used in the ADAU145x schematic. It allows user to select the parameters from DM0 or DM1.