Wiki

This version (02 Jan 2023 10:57) was approved by Jagan M.

DSP Readback Generic

Description

The DSP Readback Generic block lets allow you read a specific sample from a block of samples. The drop-down control allows you to enter the which sample be read.

The number displayed onscreen is the data value sent back from the DSP considering all the blocks to the left of the Readback block. Every time you click Read, this value will be updated with the latest from the DSP. By displaying the output value from any block, in any format desired, Readback is used chiefly for debugging, and probably will prove very handy.

Values can be read back in either hex or decimal. For the latter, you must specify what format you want the number to be displayed in. Any changes to this format will shift the decimal value of the number displayed.

Targets Supported

NameADSP-214xx(Sample)ADSP-214xx(Block)ADSP-215xx/ADSP-SC5xx(Sample)ADSP-215xx/ADSP-SC5xx(Block)
DSPReadbackGeneric No YesNo Yes


Pins

Input

NameTypeDescription
Input0AudioInput Channel 0

Output

NameTypeDescription
Output0ControlOutput channel 0


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
Sample1 1 to BlockSize Sample to read from the target from block of samples


DSP Parameters

Parameter NameDescriptionADSP-214xx/SC5xx/215xx
Samplereads the sample from targetFloat
ValueRead back value from the DSPFloat


resources/tools-software/sigmastudio/toolbox/basicdsp/dspreadbackgeneric.txt · Last modified: 25 Apr 2022 09:06 by Jagan M