Click here to return to the Basic DSP page
Conjugate Magnitude takes the Complex Signal(x + j y) of input signal and compute the magnitude (squareroot(x^2 + y^2)) of input signal and pass to output. This is a block based module.
Note:- The Context Menu “Input Source” option added to this module to select the algorithm for Complex FFT and Real FFT as shown below
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Complex Signal | Complex | Complex input signal |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 1: Real Signal | Real | Magnitude of the Complex Input Signal |
Grow algorithm not supported for the module.
Add algorithm supported for the module.
IDspSigma300(Block Schematic only)