Wiki

This version is outdated by a newer approved version.DiffThis version (01 Mar 2021 15:42) was approved by Sanjeeva Reddy.

This is an old revision of the document!


Click here to return to the BasicDSP page

Block Max and Hold

The Max and Hold is a block algorithm compares the input sample with held max value and outputs the highest value.


Input Pins

NameFormat [int/dec/float] - [control/audio]Function Description
Pin 0: Input decimal(ADAU145x)- control Reset signal to the module
Pin 1: Input decimal(ADAU145x)- audio Input signal to the module

Output Pins

NameFormat [int/dec/float] - [control/audio]Function Description
Pin 0: Output decimal(ADAU145x)- audio- audioOutput signal from the module

Grow Algorithm

The module supports growth of Input channels up to 16 and one reset pin. Add Algorithm is not supported.

GUI Controls

No GUI Controls

DSP Parameter Information

No DSP parameters

Algorithm Description

This module compares the each channel inputs samples in Block of input samples with held_max value and outputs highest value when reset is Off. Compares the each channel inputs samples in Block of input samples and outputs the highest value when reset pin is high.

Supported IC's

1. ADAU145x (IDspSigma300)

resources/tools-software/sigmastudio/toolbox/basicdsp/blockmaxandhold.1513663559.txt.gz · Last modified: 19 Dec 2017 07:05 by Sanjeeva Reddy