The information here is preliminary.
Click here to return to the SigmaStudio Algorithm Resource Summary section.
Category | Algorithm | Executed Instructions | Program RAM | DATA Ram | Parameter RAM | Description | Processors | ||
---|---|---|---|---|---|---|---|---|---|
Dynamic Mixers | Adaptive Mixer Dual (Graph) | 61 | 61 | 19 | 68 | A mixer that determines the mix ratio based on a separate user data input. | ADAU144x, ADAU176x, ADAU1781 | ||
Dynamic Mixers | Adaptive Mixer Single (Graph) | 45 | 45 | 17 | 35 | A mixer that determines the mix ratio based on a separate user data input. | ADAU144x, ADAU176x, ADAU1781 | ||
Transforms | Hilbert Transform | 97 | 97 | 60 | 26 | Outputs the real and imaginary components of the result of the Hilbert Transform performed on the input signal. | ADAU144x, ADAU176x, ADAU1781 |