Wiki

This version is outdated by a newer approved version.DiffThis version (14 Nov 2012 19:52) was approved by William Jahn.The Previously approved version (05 Nov 2012 20:05) is available.Diff

This is an old revision of the document!


SigmaStudio ADI Algorithm Resource Summary

The information here is preliminary.

Click here to return to the SigmaStudio Algorithm Resource Summary section.

CategoryAlgorithmExecuted InstructionsProgram RAMDATA RamParameter RAMDescriptionProcessors
Beam FormingAdaptive Beam Forming189189175177Uses two microphone inputs and intelligently creates a directional sensitivity pattern to focus on a source in the stereo fieldADAU144x, ADAU176x, ADAU1781
EnvelopesGeneric Gain Envelope4444915Generates a gain envelope with controllable gain vs. time.ADAU144x, ADAU176x, ADAU1781
EnvelopesGeneric Gain Envelope (Grow)2210Adds another channel to the Generic Gain Envelope block.ADAU144x, ADAU176x, ADAU1781
EnvelopesGeneric Gain Envelope Endless Loop47471016Generates a fully-programmable envelope and applies it to an input signal.ADAU144x, ADAU176x, ADAU1781
EnvelopesGeneric Gain Envelope Endless Loop (Grow)2210Adds another channel to the Generic Gain Envelope Endless Loop block.ADAU144x, ADAU176x, ADAU1781
Record AlgorithmsEnhanced Stereo Capture (ESC)2121127Takes a stereo record-signal and creates a wider stereo image.ADAU144x, ADAU176x, ADAU1781
Record AlgorithmsOffline Microphone Match4040126Calibrates the gain required to match the levels of two microphones.ADAU144x, ADAU176x, ADAU1781
Record AlgorithmsWind Noise Suppressor (With Detection Filter Outputs)1071074028Detects and suppresses wind noise. Also includes a stereo output of the low pass detection filter which can be used for debugging.ADAU144x, ADAU176x, ADAU1781
Record AlgorithmsWind Noise Suppressor1031033828Detects and suppresses wind noise.ADAU144x, ADAU176x, ADAU1781
Surround & 3D AudioMono2Stereo20203326Takes a mono signal and creates a stereo image from a single source.ADAU144x, ADAU176x, ADAU1781
Surround & 3D AudioSuperPhat Spatializer1621629052Allows for a wider stereo image to be played back from two closely spaced speakers.ADAU144x, ADAU176x, ADAU1781
Surround & 3D AudioPhat-Stereo131352Uses stereo cross-coupling to simulate surround in stereo speakers and other 2-channel situationsADAU144x, ADAU176x, ADAU1781
Surround & 3D AudioADI Surround191191346228TBDADAU144x
Surround & 3D AudioADI Virtual17617617748TBDADAU144x, ADAU176x, ADAU1781
Voice DetectorVoice Activity Detector4848155Outputs signals to be used by the VAD flag for speech detection. Must be used in conjunction with the VAD flag.ADAU144x, ADAU176x, ADAU1781
Voice DetectorVoice Activity Detector (W/ Accelerator)84842111Improved version of the Voice Activity Detector that has an accelerated reaction time after voice stops being present.ADAU144x, ADAU176x, ADAU1781
Voice DetectorVAD Flag171772Shows you if there is voice or not and must be used in conjunction with the Voice Activity Detector.ADAU144x, ADAU176x, ADAU1781
Pitch ModificationPitch Transposer76763204Shifts the pitch of the incoming signal by changing its fundamental frequency.ADAU144x, ADAU176x, ADAU1781
Pitch ModificationPitch Transposer Data Controlled76763203Shifts the pitch of the incoming signal by changing its fundamental frequency.ADAU144x, ADAU176x, ADAU1781
Dynamic BassMonoDynamic Bass Boost46462340The Dynamic Bass Boost block provides boost that varies with input-signal level: lower levels require, and receive, more bass than higher levels.ADAU144x, ADAU176x, ADAU1781
Dynamic BassMonoDynamic Bass Boost (Add Mono)462240This grows the algorithm by adding another channel to the block.ADAU144x, ADAU176x, ADAU1781
Dynamic BassMonoDynamic Bass Boost (Add Stereo)59592840This grows the algorithm by adding another two channels to the block.ADAU144x, ADAU176x, ADAU1781
Dynamic BassMonoDynamic Enhancement3737249Provides a variable bass enhancement as a function of input-signal level.ADAU144x, ADAU176x, ADAU1781
Dynamic BassMonoDynamic Enhancement (Add Mono)3737239This grows the algorithm by adding another channel to the block.ADAU144x, ADAU176x, ADAU1781
Dynamic BassMonoDynamic Enhancement (Add Stereo)4848289This grows the algorithm by adding another two channels to the block.ADAU144x, ADAU176x, ADAU1781
Dynamic BassMonoSuperbass1401405857Psychoacoustic bass enhancement algorithm that improves the perceived level of bass by amplifying higher frequency harmonics.ADAU144x, ADAU176x, ADAU1781
Dynamic BassStereoDynamic Bass Boost59592940The Dynamic Bass Boost block provides boost that varies with input-signal level: lower levels require, and receive, more bass than higher levels.ADAU144x, ADAU176x, ADAU1781
Dynamic BassStereoDynamic Bass Boost (Add Mono)46462240This grows the algorithm by adding another channel to the block.ADAU144x, ADAU176x, ADAU1781
Dynamic BassStereoDynamic Bass Boost (Add Stereo)59592840This grows the algorithm by adding another two channels to the block.ADAU144x, ADAU176x, ADAU1781
Dynamic BassStereoDynamic Enhancement4848299Provides a variable bass enhancement as a function of input-signal level.ADAU144x, ADAU176x, ADAU1781
Dynamic BassStereoDynamic Enhancement (Add Mono)3737239This grows the algorithm by adding another channel to the block.ADAU144x, ADAU176x, ADAU1781
Dynamic BassStereoDynamic Enhancement (Add Stereo)4848289This grows the algorithm by adding another two channels to the block.ADAU144x, ADAU176x, ADAU1781
Dynamic BassStereoSuperbass1751757755Psychoacoustic bass enhancement algorithm that improves the perceived level of bass by amplifying higher frequency harmonics.ADAU144x, ADAU176x, ADAU1781
Dynamic BassStereoSuperbass (Slew Optimized)1631637257Psychoacoustic bass enhancement algorithm that improves the perceived level of bass by amplifying higher frequency harmonics. Includes slewing.ADAU144x, ADAU176x, ADAU1781
EffectsVocal Chorus23423481179Produces an effect where the audio signal is given multiple delays to enrich and thicken the sound, like several voices (or instruments) playing at once.ADAU144x, ADAU176x
EffectsReverb339339507885Simulates the natural reverberation of an echoic space, such as a performance hall, and mixes it back into the original sound.ADAU144x,
LoudnessLoudness (Low and High)7171278A volume control that corrects its frequency response for equal-loudness, based on the Fletcher and Munson equal-loudness curves.ADAU144x, ADAU176x, ADAU1781
UnclassifiedAutomatic Volume Control1231235649A volume control that adapts to the input signal level and attempts to keep the output level of the system fairly constant.ADAU144x, ADAU176x, ADAU1781
Noise RemovalNoise Reduction6066062272269Breaks the input signal into many frequency bands and suppresses bands where no signal is present, therefore reducing noise.ADAU144x, ADAU176x
resources/tools-software/sigmastudio/toolbox/adialgorithmsresourcetable.1352919146.txt.gz · Last modified: 14 Nov 2012 19:52 by William Jahn