Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:sigmastudio:toolbox:adialgorithmsresourcetable [14 Nov 2012 19:52]
William Jahn ADI surround
resources:tools-software:sigmastudio:toolbox:adialgorithmsresourcetable [15 Nov 2012 21:03]
William Jahn Fixed Pitch Transposer links
Line 23: Line 23:
 |Voice Detector|||[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​voiceactivitydetector|Voice Activity Detector]] (W/ Accelerator)|84|84|21|11|Improved version of the Voice Activity Detector that has an accelerated reaction time after voice stops being present.|ADAU144x,​ ADAU176x, ADAU1781| |Voice Detector|||[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​voiceactivitydetector|Voice Activity Detector]] (W/ Accelerator)|84|84|21|11|Improved version of the Voice Activity Detector that has an accelerated reaction time after voice stops being present.|ADAU144x,​ ADAU176x, ADAU1781|
 |Voice Detector|||[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​vadflag|VAD Flag]]|17|17|7|2|Shows you if there is voice or not and must be used in conjunction with the Voice Activity Detector.|ADAU144x,​ ADAU176x, ADAU1781| |Voice Detector|||[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​vadflag|VAD Flag]]|17|17|7|2|Shows you if there is voice or not and must be used in conjunction with the Voice Activity Detector.|ADAU144x,​ ADAU176x, ADAU1781|
-|Pitch Modification|||[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​pitchtransposer|Pitch Transposer]]|76|76|320|4|Shifts the pitch of the incoming signal by changing its fundamental frequency.|ADAU144x,​ ADAU176x, ADAU1781| +|Pitch Modification|||[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​pitchmodification/​pitchtransposer|Pitch Transposer]]|76|76|320|4|Shifts the pitch of the incoming signal by changing its fundamental frequency.|ADAU144x,​ ADAU176x, ADAU1781| 
-|Pitch Modification|||[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​pitchtransposer|Pitch Transposer]] Data Controlled|76|76|320|3|Shifts the pitch of the incoming signal by changing its fundamental frequency.|ADAU144x,​ ADAU176x, ADAU1781|+|Pitch Modification|||[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​pitchmodification/​pitchtransposer|Pitch Transposer]] Data Controlled|76|76|320|3|Shifts the pitch of the incoming signal by changing its fundamental frequency.|ADAU144x,​ ADAU176x, ADAU1781|
 |Dynamic Bass||Mono|[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​dynamicbassboost|Dynamic Bass Boost]]|46|46|23|40|The Dynamic Bass Boost block provides boost that varies with input-signal level: lower levels require, and receive, more bass than higher levels.|ADAU144x,​ ADAU176x, ADAU1781| |Dynamic Bass||Mono|[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​dynamicbassboost|Dynamic Bass Boost]]|46|46|23|40|The Dynamic Bass Boost block provides boost that varies with input-signal level: lower levels require, and receive, more bass than higher levels.|ADAU144x,​ ADAU176x, ADAU1781|
 |Dynamic Bass||Mono|[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​dynamicbassboost|Dynamic Bass Boost]] (Add Mono)|46||22|40|This grows the algorithm by adding another channel to the block.|ADAU144x,​ ADAU176x, ADAU1781| |Dynamic Bass||Mono|[[resources/​tools-software/​sigmastudio/​toolbox/​adialgorithms/​dynamicbassboost|Dynamic Bass Boost]] (Add Mono)|46||22|40|This grows the algorithm by adding another channel to the block.|ADAU144x,​ ADAU176x, ADAU1781|
resources/tools-software/sigmastudio/toolbox/adialgorithmsresourcetable.txt · Last modified: 15 Nov 2012 21:03 by William Jahn