Click here to return to the ADI Algorithms page
Vocal Chorus produces an effect where the audio signal is given multiple delays to enrich and thicken the sound, like several voices (or instruments) playing at once. The delay time is modulated by a low-frequency oscillator (LFO) to achieve a shimmering, spacious effect due to a combination of beat frequencies and the slight pitch-bending that occurs as the delay time is changed.
This cell is intended chiefly for voice.
After the default algorithm has been established, this cell is able to have other algorithms added to it. Right-click the cell and select Add Algorithm > IC N > Reverb, which will add another pair of stereo inputs/outputs. (If you are using more than one DSP processor, you will need to add an algorithm for the desired IC.)