This is an old revision of the document!
Click here to return to the Pitch Modification page
This algorithm shifts the frequency of an incoming signal. The frequency shift is “voltage-controlled”, meaning that there is an input pin that controls the pitch shift amount based on its value. See Pitch Transposer page for GUI/RAM controlled version. | ![]() |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Input | any - any | Input signal that will have its frequency shifted |
Pin 1: Input | either | Frequency shift amount (percentage/sampling-rate) |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Output | any - any | Outputs the processed signal |
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Delay Reserved | 300 | [2.0:Max Data RAM Available] | This control sets the number of samples of audio delay that are reserved in memory as a buffer used for the pitch shifting algorithm. Smaller delay buffers result in more discontinuities in the pitch shifted output signal, which causes some harmonic distortion. Setting this delay buffer to a very large size will result in less distortion, but at the cost of increased delay memory usage. |
The algorithm takes an input signal and shifts it in frequency up or down depending on the value of the the frequency shift control signal. The control input value should be the shift percentage divided by the sampling rate, for example for a shift of +100%: control signal = (100 / 48000) = 0.0020833 (fixed-point)
Here is a time-domain display of a sine tone being shifted in frequency. The top sine tone is the input signal, and the bottom sine tone is the output.
Approximate Output frequency = Input frequency + (Input frequency * (Delay Reserved x 0.001) x shift(%))
For example, consider the following schematic,
Here,
Shift = 0.38 (38%)
Input frequency = 100 Hz
Delay Reserved = 960
control signal = 38/48000 ⇒ 0.000791667
Approximate Output frequency = 100 + (100 * (960 x 0.001) x 0.38) = 136.48
Here is the same example in the frequency domain. This picture shows the frequency domain of the input signal.
This picture shows the frequency domain of the output signal.
Toolbox Path | ADI Algorithms/Pitch Modification |
Cores Supported | AD194x ADAU170x ADAU144x ADAU176x ADAU1781 ADAU145X |
“Grow Algorithm” Supported | no |
“Add Algorithm” Supported | no |
Subroutine/Loop Based | no |
Program RAM | 76 |
Data RAM | 1019 |
Parameter RAM | 4 |