This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:toolbox:adialgorithms:pitchmodification:pitchtransposerdatacontrolled [11 Aug 2020 13:44] – Added more details Venkatesan Krishnamoorthy | resources:tools-software:sigmastudio:toolbox:adialgorithms:pitchmodification:pitchtransposerdatacontrolled [04 Jan 2021 06:40] (current) – Updated for Pitch Transfer Memory used for option Sanjeeva Reddy | ||
---|---|---|---|
Line 19: | Line 19: | ||
^GUI Control Name^Default Value^Range^Function Description^ | ^GUI Control Name^Default Value^Range^Function Description^ | ||
|Delay Reserved|300|[2.0: | |Delay Reserved|300|[2.0: | ||
+ | |||
+ | === Context Menu === | ||
+ | Right-click on the module to open the context menu window. By default, DM1 memory is used for delay. User can choose either DM0,DM1 or PM for Delay. Change in memory used for delay leads to re-compile the project(supports for ADAU145x/ | ||
+ | \\ | ||
+ | {{ : | ||
+ | \\ | ||
===Algorithm Description=== | ===Algorithm Description=== |