This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:sigmastudio:toolbox:adialgorithms:pitchmodification:pitchtransposerdatacontrolled [11 Aug 2020 13:44] Venkatesan Krishnamoorthy Added more details |
resources:tools-software:sigmastudio:toolbox:adialgorithms:pitchmodification:pitchtransposerdatacontrolled [04 Jan 2021 06:40] Sanjeeva Reddy Updated for Pitch Transfer Memory used for option |
||
---|---|---|---|
Line 19: | Line 19: | ||
^GUI Control Name^Default Value^Range^Function Description^ | ^GUI Control Name^Default Value^Range^Function Description^ | ||
|Delay Reserved|300|[2.0:Max Data RAM Available]|This control sets the number of samples of audio delay that are reserved in memory as a buffer used for the pitch shifting algorithm. Smaller delay buffers result in more discontinuities in the pitch shifted output signal, which causes some harmonic distortion. Setting this delay buffer to a very large size will result in less distortion, but at the cost of increased delay memory usage.| | |Delay Reserved|300|[2.0:Max Data RAM Available]|This control sets the number of samples of audio delay that are reserved in memory as a buffer used for the pitch shifting algorithm. Smaller delay buffers result in more discontinuities in the pitch shifted output signal, which causes some harmonic distortion. Setting this delay buffer to a very large size will result in less distortion, but at the cost of increased delay memory usage.| | ||
+ | |||
+ | === Context Menu === | ||
+ | Right-click on the module to open the context menu window. By default, DM1 memory is used for delay. User can choose either DM0,DM1 or PM for Delay. Change in memory used for delay leads to re-compile the project(supports for ADAU145x/ADAU146x). | ||
+ | \\ | ||
+ | {{ :resources:tools-software:sigmastudio:toolbox:adialgorithms:pitchmodification:pitchtransfermemdelay.jpg?nolink |}} | ||
+ | \\ | ||
===Algorithm Description=== | ===Algorithm Description=== |