This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:adialgorithms:automaticvolumecontrol [25 Jul 2014 22:25] – add adau145x information John McCarty | resources:tools-software:sigmastudio:toolbox:adialgorithms:automaticvolumecontrol [01 Sep 2016 06:33] (current) – prasanna thirumaleshwara | ||
---|---|---|---|
Line 14: | Line 14: | ||
|Max Gain (dB)|12|0 - 15|The maximum gain that will be applied to a quiet signal as the algorithm attempts to maintain a target output level.| | |Max Gain (dB)|12|0 - 15|The maximum gain that will be applied to a quiet signal as the algorithm attempts to maintain a target output level.| | ||
|Output Level (dB)|-18|-18 to -3|The target output level (in RMS) that the algorithm will try to maintain.| | |Output Level (dB)|-18|-18 to -3|The target output level (in RMS) that the algorithm will try to maintain.| | ||
- | |Freeze Level (dB)|-36|-36 to -20|The threshold below which the algorithm considers a signal to be " | + | |Freeze Level (dB)|-36|-36 to -20|The threshold below which the algorithm considers a signal to be " |
\\ | \\ | ||
**NOTE:** this algorithm introduces a constant delay to the audio signal regardless of the AVC Enable setting. | **NOTE:** this algorithm introduces a constant delay to the audio signal regardless of the AVC Enable setting. |