This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:sigmastudio:toolbox:adialgorithms:automaticvolumecontrol [18 Feb 2013 16:50] – Added GUI controls table and example Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:adialgorithms:automaticvolumecontrol [25 Jul 2014 22:25] – add adau145x information John McCarty | ||
---|---|---|---|
Line 16: | Line 16: | ||
|Freeze Level (dB)|-36|-36 to -20|The threshold below which the algorithm considers a signal to be " | |Freeze Level (dB)|-36|-36 to -20|The threshold below which the algorithm considers a signal to be " | ||
\\ | \\ | ||
+ | **NOTE:** this algorithm introduces a constant delay to the audio signal regardless of the AVC Enable setting. | ||
+ | \\ | ||
+ | |||
+ | **ADAU145x DSP:** The ADAU145x implementation of this algorithm supports growing the input channels for 5.1/7.1 applications. However, the volume detection is calculated from the first 2 inputs only (left and right) and the resulting level compensation and delay is applied to all other channels. | ||
+ | \\ | ||
+ | \\ | ||
+ | |||
===Example=== | ===Example=== | ||
The following example test circuit shifts the AVC's input between two tone levels 20dB apart: | The following example test circuit shifts the AVC's input between two tone levels 20dB apart: |