ADAU1701
This guide refers to the pre-2007 version of the ADAU1701 evaluation board. It will be updated soon. For updated user guide information, check here: UG-072.pdf.
Launch SigmaStudio and create a new project. The Hardware Configuration tab and workspace will display.
Drag a DSPSigma100, E2Prom, and an EvalBoard100 block into the workspace.
Connect the EvalBoard100 to the DSPSigma100 block by clicking and dragging from the top blue output pin to the green input pin.
Connect the DSPSigma100 bottom blue output pin to the green input pin on the E2Prom block.
The result should look something like this:
Click Schematic (tab at the top of workspace).
Click IO in the Toolbox and drag an Input block to the workspace.
Click Volume Controls in the Toolbox and drag a Single Volume Control to the workspace.
Right-click that block (called Single 1) and choose Add Algorithm → IC1 → Gain (no slew). (This adds input / output.)
Connect the Input block’s blue output pins to the green input pins on the Volume Control.
Click IO in the Toolbox and drag two Output blocks to the workspace.
If your speakers aren’t connected to outputs 0/1, use the dropdown to change them to the correct outputs.
Connect the Volume Control blue output pins to the green input pins on the Output blocks.
After ensuring that your board is powered and connected to the PC, click Link-Compile-Download on the taskbar.
Assuming the project compiled without error, you will be in Ready-Download mode and see something similar to this figure.