Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Last revisionBoth sides next revision
resources:tools-software:sigmastudio:faq [27 Dec 2022 11:11] Sakthivel Perumalresources:tools-software:sigmastudio:faq [05 Jan 2023 08:14] – [Modules Q & A] Sowmya devi R
Line 609: Line 609:
  
 A: Algorithm Designer can be used to create custom plugin module to link the 3rd party library modules by writing the wrapper functions for accessing the library function. A: Algorithm Designer can be used to create custom plugin module to link the 3rd party library modules by writing the wrapper functions for accessing the library function.
 +
 +**Q: Why the “Generate Assembly” buttons not working in SigmaStudio for SHARC Algorithm Designer for Custom plugin generation?**
 +
 +A: The Algorithm design form should have at least 1 control to generate the assembly. We should at least add a label control into the Algorithm design form.
 +
 +**Q: Why is parameter tuning not working for custom plugin?**
 +
 +A:
 +  * Default parameters should be added into the custom plugin .xml file
 +  * Runtime parameters should be added in algorithm designer
 +\\
 +{{:resources:tools-software:sigmastudio:image2023-1-5_11-32-46.png?400}}\\
 +\\
 +  * The runtime parameter should be assigned to default parameters as shown below,
 +\\
 +{{:resources:tools-software:sigmastudio:image2023-1-5_11-51-58.png?400|}}\\
 +\\
 +  * The runtime parameter should be assigned to UI controls as shown below,
 +Step 1: Select and right click on the UI control, click on “Assign” option
 +\\
 +{{:resources:tools-software:sigmastudio:image2023-1-5_11-52-38.png?400|}}\\
 +\\
 +Step 2: In Control Action drop down select “ValueChanged”
 +\\
 +{{:resources:tools-software:sigmastudio:image2023-1-5_11-53-54.png?400|}}\\
 +\\
 +Step 3: Select the runtime parameter for corresponding UI control and click on apply
 +\\
 +{{:resources:tools-software:sigmastudio:image2023-1-5_11-54-38.png?400|}}\\
 +\\
 +Step 4: Review the UI control settings in properties window for Minimum, Maximum, Values
 +\\
 +{{:resources:tools-software:sigmastudio:image2023-1-5_11-55-35.png?400|}}\\
 +\\
 +These steps to be followed for every UI control to avoid runtime parameter tuning issues.
  
 ====== SigmaStudio for SHARC Host Packeting Q & A ====== ====== SigmaStudio for SHARC Host Packeting Q & A ======
resources/tools-software/sigmastudio/faq.txt · Last modified: 15 Feb 2023 13:34 by Sakthivel Perumal