Wiki

This version (14 Jun 2012 22:16) was approved by Brett Gildersleeve.The Previously approved version (14 Jun 2012 19:19) is available.Diff

Script Dialog

Click here to return to the Dialogs page

SigmaStudio includes a script-able automation engine allowing control over most common application operations. To access the Script dialog, select Tools - Script… in the main application menu or press F12.

Scripting in both the C# and Visual Basic languages is supported. For more information about the SigmaStudio Script engine check the detailed documentation in the attached PDF: sigmastudio_scripting.pdf




SigmaStudioServer:

SigmaStudioServer is an automation interface for SigmaStudio that allows external software applications to control or automate SigmaStudio functions. (For example, National Instruments LabVIEW) The server interface library Analog.SigmaStudioServer.dll implements Microsoft .Net and ActiveX server interfaces. For more information or detailed documentation please contact Analog Devices on the SigmaDSP Community on EngineerZone.

resources/tools-software/sigmastudio/developmentenvironment/script.txt · Last modified: 14 Jun 2012 22:16 by Brett Gildersleeve