Wiki

This version (13 Jun 2012 22:26) was approved by William Jahn.

Schematic Tab


Click here to return to the Development Environment page

Once the hardware configuration is set, you are ready to construct a DSP design. Designs are created in the Schematic tab workspace (Figure 1). The Toolbox at the left gives access to various libraries containing building blocks that can be dragged and dropped in the schematic workspace on the right.

Note: The Schematic Tab is not displayed until a programmable DSP IC is inserted in the Hardware Configuration tab.



Schematic designs can be organized into multiple layers called Hierarchy Boards. The design example in Figure 1 has a single hierarchy layer called 'Main', as shown in the tab at the bottom of the screen. 'Main' is the default layer created for all designs and cannot be renamed. For more information on Hierarchy Boards and how to organize your program flow into board layers see the Hierarchy Board topic.

Where to go now

If you're ready to begin designing, refer to the following sections for more information:

  • To set up a simple application, skip to Tutorials and follow the examples for Stereo Audio with Volume Control and 5-band EQ and Probe and Stimulus Blocks.
  • Learn about individual blocks and their functions in the Schematic Toolbox section, example schematics, and get detailed information about the algorithms represented by the blocks.
  • For advanced operations and control of the hardware, take a look at the Hardware Windows section.
  • Learn more about general SigmaStudio functions in Using SigamStudio, and see detailed information about microcontroller considerations in Basic SigmaDSP Architecture.
resources/tools-software/sigmastudio/developmentenvironment/schematictab.txt · Last modified: 03 Jan 2013 20:42 (external edit)