This shows you the differences between two versions of the page.
resources:tools-software:sigmastudio:developmentenvironment:hardware_windows:e2promwindow [15 Jun 2012 15:10] William Jahn created |
resources:tools-software:sigmastudio:developmentenvironment:hardware_windows:e2promwindow [15 Jun 2012 15:11] William Jahn updated picture formatting |
||
---|---|---|---|
Line 12: | Line 12: | ||
- To use the E2Prom, insert the E2Prom IC block into [[resources/tools-software/sigmastudio/developmentenvironment/hardwareconfigurationtab|Hardware Configuration Tab]] and connect it to the USB communication channel block as show in the figure below. | - To use the E2Prom, insert the E2Prom IC block into [[resources/tools-software/sigmastudio/developmentenvironment/hardwareconfigurationtab|Hardware Configuration Tab]] and connect it to the USB communication channel block as show in the figure below. | ||
- | - {{e2prompic1.png}} | + | - {{ e2prompic1.png }} |
- Compile/Link/Download the project and verify that "Ready - Download" is displayed on the status bar. | - Compile/Link/Download the project and verify that "Ready - Download" is displayed on the status bar. | ||
- To download the compiled project's program data to the E2Prom, Right-Click on the DSP block in the Hardware Configuration window and select** Write Latest Compilation to E2PROM** from the menu. Note if your E2Prom's size differs from the default 16kB size, you should first adjust the size setting in the Read/Write window (see below) before writing . | - To download the compiled project's program data to the E2Prom, Right-Click on the DSP block in the Hardware Configuration window and select** Write Latest Compilation to E2PROM** from the menu. Note if your E2Prom's size differs from the default 16kB size, you should first adjust the size setting in the Read/Write window (see below) before writing . | ||
- | - {{e2prompic2.png}} | + | - {{ e2prompic2.png }} |
- If your hardware is setup correctly, you should see the Download E2Prom progress dialog. | - If your hardware is setup correctly, you should see the Download E2Prom progress dialog. | ||
- | - {{e2prompic3.png}} | + | - {{ e2prompic3.png }} |
-------------------------------------------------------------------------------- | -------------------------------------------------------------------------------- | ||
Line 25: | Line 25: | ||
To open the E2Prom Read/Write window, Click the WinE2PromLoader tab at the bottom of the Hardware Configuration window or Right-click on the E2Prom IC block and select Read/Write Window from the menu. | To open the E2Prom Read/Write window, Click the WinE2PromLoader tab at the bottom of the Hardware Configuration window or Right-click on the E2Prom IC block and select Read/Write Window from the menu. | ||
\\ | \\ | ||
- | {{e2prompic5.png}} | + | {{ e2prompic5.png }} |
\\ | \\ | ||
\\ | \\ |