Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Last revisionBoth sides next revision
resources:tools-software:sharc-audio-module:baremetal:matlab_volume_control [19 Aug 2019 22:06] Chad Wentworthresources:tools-software:sharc-audio-module:baremetal:matlab_volume_control [19 Aug 2019 22:11] – [Generating C Code with Matlab Coder] Chad Wentworth
Line 54: Line 54:
   - Now the code can be generated   - Now the code can be generated
   - **Build type** should be set to **Source Code**   - **Build type** should be set to **Source Code**
-  - **Language** should be **C++**+  - **Language** should be **C plus plus**
   - Change **Hardware Board** to **None - Select device below**   - Change **Hardware Board** to **None - Select device below**
   - **Device vendor** should be **Analog Devices**   - **Device vendor** should be **Analog Devices**
resources/tools-software/sharc-audio-module/baremetal/matlab_volume_control.txt · Last modified: 19 Aug 2019 22:26 by Chad Wentworth