This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:sharc-audio-module:baremetal:matlab_volume_control [19 Aug 2019 22:06] – Chad Wentworth | resources:tools-software:sharc-audio-module:baremetal:matlab_volume_control [19 Aug 2019 22:11] – [Generating C Code with Matlab Coder] Chad Wentworth | ||
---|---|---|---|
Line 54: | Line 54: | ||
- Now the code can be generated | - Now the code can be generated | ||
- **Build type** should be set to **Source Code** | - **Build type** should be set to **Source Code** | ||
- | - **Language** should be **C++** | + | - **Language** should be **C plus plus** |
- Change **Hardware Board** to **None - Select device below** | - Change **Hardware Board** to **None - Select device below** | ||
- **Device vendor** should be **Analog Devices** | - **Device vendor** should be **Analog Devices** |