This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sharc-audio-module:baremetal:matlab_pitchshift [29 Apr 2020 19:22] – [Executing the Code in CCES] Chad Wentworth | resources:tools-software:sharc-audio-module:baremetal:matlab_pitchshift [28 May 2020 22:42] (current) – [Create Project in CrossCore Embedded Studio] Chad Wentworth | ||
---|---|---|---|
Line 83: | Line 83: | ||
====Create Project in CrossCore Embedded Studio==== | ====Create Project in CrossCore Embedded Studio==== | ||
- | Use the Bare Metal Project Wizard to create a project that the MATLAB generated code can be integrated into. | + | Use the Bare Metal Project Wizard to create a project that the MATLAB generated code can be integrated into. Using all the default settings in the wizard will create a working 3 core project. |
<note tip> | <note tip> |