This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:sharc-audio-module:baremetal:downloading-and-installing [18 Jan 2019 18:44] Chad Wentworth |
resources:tools-software:sharc-audio-module:baremetal:downloading-and-installing [03 Jan 2021 21:43] Robin Getz fix links |
||
---|---|---|---|
Line 15: | Line 15: | ||
- After completing this operation, you should see three folders appear in the Project Explorer. Each project corresponds to each of the three cores on the ADSP-SC589. Core 0 is the ARM core. Cores 1 and 2 are the two SHARC cores. By default, the project is configured to pass audio from the 1/8" audio input jack to the 1/8" audio output jack. Build the project and create a debug profile for the JTAG emulator you’re using (ICE1000 or ICE2000). From here, you’ll be able to download and run the project on the ADSP-SC589. | - After completing this operation, you should see three folders appear in the Project Explorer. Each project corresponds to each of the three cores on the ADSP-SC589. Core 0 is the ARM core. Cores 1 and 2 are the two SHARC cores. By default, the project is configured to pass audio from the 1/8" audio input jack to the 1/8" audio output jack. Build the project and create a debug profile for the JTAG emulator you’re using (ICE1000 or ICE2000). From here, you’ll be able to download and run the project on the ADSP-SC589. | ||
<note>JP1 on the SHARC Audio Module should be removed (disconnected) when using an emulator to connect to the board</note> | <note>JP1 on the SHARC Audio Module should be removed (disconnected) when using an emulator to connect to the board</note> | ||
- | * For more information on connecting an emulator, see the [[http://www.analog.com/media/en/dsp-documentation/evaluation-kit-manuals/ICE_emu_1000_2000_rev_manual.pdf|ICE-1000/ICE-2000 Emulator User's Guide]]. | + | * For more information on connecting an emulator, see the [[adi>media/en/dsp-documentation/evaluation-kit-manuals/ICE_emu_1000_2000_rev_manual.pdf|ICE-1000/ICE-2000 Emulator User's Guide]]. |
- | * For more information on setting up the debug profile, see [[http://www.analog.com/en/education/education-library/videos/1831703659001.html|Debugging on a Hardware Target with CCES]] | + | * For more information on setting up the debug profile, see [[adi>en/education/education-library/videos/1831703659001.html|Debugging on a Hardware Target with CCES]] |
<note>The default CCES license provided with the SHARC Audio Module SDK is not a full CCES license; it only enables debug sessions for ICE-1000 emulators.</note> | <note>The default CCES license provided with the SHARC Audio Module SDK is not a full CCES license; it only enables debug sessions for ICE-1000 emulators.</note> | ||