Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:sharc-audio-module:baremetal:configuring-the-framework [18 Jan 2019 18:48] – [Configuring the Framework] Chad Wentworthresources:tools-software:sharc-audio-module:baremetal:configuring-the-framework [06 Mar 2019 17:56] (current) – [4. Enabling and Configuring A2B Support] Chad Wentworth
Line 143: Line 143:
 If the SHARC Audio Module is the A2B bus master, there are a number of fixed network topologies that can be used.  These network topologies are essentially A2B initialization sequences that will initialize the various I2C components on the slave nodes on the A2B bus.  Only one A2B topology can be selected at a time. If the SHARC Audio Module is the A2B bus master, there are a number of fixed network topologies that can be used.  These network topologies are essentially A2B initialization sequences that will initialize the various I2C components on the slave nodes on the A2B bus.  Only one A2B topology can be selected at a time.
  
-If you'd like to create your own A2B topologies, see the tutorial on this topic.+If you'd like to create your own A2B topologies, see the [[resources:tools-software:sharc-audio-module:baremetal:driver-creation-tutorial|tutorial]] on this topic.
  
 <code c> <code c>
resources/tools-software/sharc-audio-module/baremetal/configuring-the-framework.txt · Last modified: 06 Mar 2019 17:56 by Chad Wentworth