Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:sharc-audio-module:baremetal:baremetal-framework-architecture [14 Nov 2018 03:11] Chad Wentworthresources:tools-software:sharc-audio-module:baremetal:baremetal-framework-architecture [18 Jan 2019 18:47] (current) – [Baremetal Framework Project Structure] Chad Wentworth
Line 1: Line 1:
 ===== Baremetal Framework Project Structure ===== ===== Baremetal Framework Project Structure =====
-<WRAP round 65% tip+ 
-Helpful video: [[https://www.analog.com/en/education/education-library/videos/5858377449001.html|The Structure of the Bare Metal Framework]] +{{youtube>uAER53AcOco?medium}} 
-</WRAP>+
 There are three distinct Project folders which each correspond to the code running on a distinct processor core of the ADSP-SC589. Furthermore, there are some folders which contain code that is shared between the three cores. There are three distinct Project folders which each correspond to the code running on a distinct processor core of the ADSP-SC589. Furthermore, there are some folders which contain code that is shared between the three cores.
  
resources/tools-software/sharc-audio-module/baremetal/baremetal-framework-architecture.txt · Last modified: 18 Jan 2019 18:47 by Chad Wentworth