This is an old revision of the document!
This section will take you through a few examples to set up and run audio, including using the shell terminal program to interface with the application and stream audio via a .wav file.
Follow the instructions below to set up your specific hardware variant.
TODO
Follow the instructions below to set up the software.
This tutorial uses TeraTerm as the serial interface to your hardware.
Follow the instructions below to set up a connection to your hardware:
This section will instruct the user how to transfer a WAV file to the SHARC Audio platform over XMODEM. The example will use TeraTerm to send the WAV file.
This setup will allow audio to pass from input to output through your hardware by using both an analog input source and an analog output source. This setup allows us to play audio via an Audio Jack from a phone and output to a mini portable speaker.