Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:sharc-audio-module:advanced-audio-projects:examples-analog-audio [19 Sep 2023 19:41] Rebecca Butlerresources:tools-software:sharc-audio-module:advanced-audio-projects:examples-analog-audio [21 Sep 2023 22:18] (current) – [Serial Terminal Setup] Sagar Vaidya
Line 20: Line 20:
  
 ==== EV-SC594-SOM + Carrier ==== ==== EV-SC594-SOM + Carrier ====
-TODO+| 1. Power on your SOM board by pluggin in the 12V Power Supply to the 12V connector on the career board. If the board is properly powered, the green PWR LED on the SOM board will light up. | {{:resources:tools-software:sharc-audio-module:advanced-audio-projects:som_pwr.jpg?400|}}| 
 +| 2. Plug the USB Micro Type C side to the SOM board USB connector and the USB Type A side to a USB connection on the PC. | {{:resources:tools-software:sharc-audio-module:advanced-audio-projects:som_usb.jpg?400|}}| 
 +| 3. Connect the 3.5mm stereo audio cable to an audio source with audio jack support (such as a cell phone) and to the AN1/2 connector on the career board. Connect the Portable speaker to the HEADPHONES connector on the career board (ensure the speaker is turned on!). | {{:resources:tools-software:sharc-audio-module:advanced-audio-projects:som_aud.jpg?400|}}| 
 +| 4. Proceed to the software setup instructions //(common for all hardware variants)//| NA| 
  
 ---- ----
Line 32: Line 36:
  
 **Follow the instructions below to set up a connection to your hardware:** **Follow the instructions below to set up a connection to your hardware:**
-| 1. Open TeraTerm and connect to a new Serial Session, connecting to the Port labeled //SC5xx Communications Port//.| {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example1.png?400 |}}  {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example2.png?400 |}} |+| 1. Open TeraTerm and connect to a new Serial Session, connecting to the Port labeled //SC5xx Communications Port// or //FTDI COMxx Port//.| {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example1.png?400 |}}  {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example2.png?400 |}} OR {{:resources:tools-software:sharc-audio-module:advanced-audio-projects:som_serial.jpg?400|}}|
 | 2. After connection, navigate to the //Serial Port// settings under //Setup// and change the Port settings to the following: \\ \\ //Speed/Baud - 115200// \\ //Data Bits - 8-bit// \\ //Stop Bits - 1// \\ //Parity - None// \\ //Flow Control - None//  | {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example4.png?400 |}}  {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example3.png?400 |}} | | 2. After connection, navigate to the //Serial Port// settings under //Setup// and change the Port settings to the following: \\ \\ //Speed/Baud - 115200// \\ //Data Bits - 8-bit// \\ //Stop Bits - 1// \\ //Parity - None// \\ //Flow Control - None//  | {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example4.png?400 |}}  {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example3.png?400 |}} |
 | 3. With a successful connection, after reset, the terminal will display //SAM Audio Starter// with the version. Type //help// to list the available shell commands. | {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example5.png?400 |}} {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example6.png?400 |}}  | | 3. With a successful connection, after reset, the terminal will display //SAM Audio Starter// with the version. Type //help// to list the available shell commands. | {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example5.png?400 |}} {{ :resources:tools-software:sharc-audio-module:advanced-audio-projects:example6.png?400 |}}  |
resources/tools-software/sharc-audio-module/advanced-audio-projects/examples-analog-audio.txt · Last modified: 21 Sep 2023 22:18 by Sagar Vaidya