Below is a list of common problems faced during setup and their solutions or workarounds. Note that some of these may be bugs that are planned (or not) to be fixed and some of them are items commonly missed during setup.
Issue Description When attempting to flash the bootloader(s) on the ADZS-SC589-MINI using the CLDP the device returns Error: failed erasing affected sectors. | ![]() |
Applies to hardware versions ADZS-SC589-MINI v1.5 ADZS-SC589-MINI v2.1 | |
Root Cause There is a mismatch between the external flash byte addressing mode between the application/bootloader and the DXE flasher used to re-flash via CLDP, therefore the CLDP command cannot complete the erasing/flash process. | |
Workaround Steps/Solution 1. Remove the JP1 jumper header. 2. Reset the board either by the reset button or by a power cycle. 3. Re-flash bootloader0 using the instructions program-flash. 4. Repeat steps for bootloader1, leaving JP1 disconnected. 5. After bootloader flashing is complete, replace JP1 back to positions 1-2 to proceed to application flashing. | ![]() |
Planned fix status - Backlogged |
Issue Description When attempting to flash the application(s) on the ADZS-SC589-MINI using the SAM Flasher, or when attempting to connect to the terminal via the shell (TeraTerm), the SC5xx port does not show up in the drop-down list. | ![]() |
Applies to hardware versions ADZS-SC589-MINI - all versions | |
Root Cause The device is not powered on OR the JP1 jumper has not been placed back into the 1-2 position OR the .inf file has not been installed in the device drivers in Windows. | ![]() |
Workaround Steps/Solution Follow the steps described in environment_setup under CLD CDC USB Driver Setup to install the CLD CDC Driver (Note this is required for the USB/OTG to become operational. | |
Planned fix status - N/A |
Issue Description When attempting to flash the application via the SAM flasher, the SC5xx port shows up, but returns an invalid serial port status when pressing the Update button. | ![]() |
Applies to hardware versions ADZS-SC589-MINI - all versions | |
Root Cause The device is not running in the bootloader and is currently attached to the application. | ![]() |
Workaround Steps/Solution The device needs to be running in bootloader mode to flash a new application. There will be a separate SC5xx Communications port that appears that is separate from the port that appears in application mode. Follow the steps outlined in program-flash under Application Flash via SAM Flasher to enter the bootloader and proceed to the application flash. | |
Planned fix status - N/A |
Issue Description After following the steps for the ADZS-SC589-MINI to flash the bootloader and application, the application doesn't appear to boot. LED10 blinks twice and then there are no additional LED blinks. | |
Applies to hardware versions ADZS-SC589-MINI - v2.1 - 1.0.0-Github and Networking-1.0.0-Github | |
Root Cause The device is running with an incorrect core clock (500MHz) that is out of bounds for the part given the core voltage configured for v2.1. This can cause intermittent failures for the application to run and can apply to certain batches of hardware that are more sensitive to this clock setting. | ![]() |
Workaround Steps/Solution The device needs to run at a lower core clock of 450MHz Follow the steps below to adjust the application code. 1. Navigate to the directory ALL/include and open up clocks.h. 2. Modify CCLK to 450000000. 3. Navigate to the directory ARM/include and open up FreeRTOSConfig.h 4. Modify configCPU_CLOCK_HZ to 450000000 5. Recompile and reflash the program according to program-flash under Application Flash via SAM Flasher | ![]() ![]() |
Planned fix status - Fixed |
Issue Description After following the steps for the ADZS-SC589-MINI to run a debug session, doesn't blink the LEDs. We also cannot connect to the shell termainal. When the debugger is paused, it almost always pauses in the adi_os_vectors_start code. | ![]() |
Applies to hardware versions All hardware/branches that support FreeRTOS | |
Root Cause See root cause details here: https://interactive.freertos.org/hc/en-us/community/posts/115002374012-Analog-Devices-ADSP-SC5xx-Cortex-A5-using-CrossCore-Embedded-Studio-GCC- | |
Workaround Steps/Solution Ensure that Enable Semihosting is Unchecked as described in debug-session | ![]() |
Planned fix status - No plan |