Wiki

This version is outdated by a newer approved version.DiffThis version (22 May 2023 19:01) was approved by Rebecca Butler.The Previously approved version (22 May 2023 17:41) is available.Diff

This is an old revision of the document!


Appendix A

Below are matrices of software and hardware compatibilities.

Overview

The advanced audio projects support several different feature sets and software versions, along with different versions of hardware, which allows for flexibility across various use-cases.

Hardware Compatibility

Below are the hardware and versions of hardware that the software has been tested on. Other versions of the hardware may be supported but they have not been verified. This list may be expanded if users find additional compatibility.

Hardware ADZS-SC589-MINI ADZS-SC584-EZLITE EV-SC594-SOM + EV-SOMCCR-EZKIT
Version(s) v1.4 v2.4 SOM Rev C
v1.5 Carrier Rev A

Software Compatibility

Below is a list with links to the versions of software available publicly for each hardware kit.

Software ADZS-SC589-MINI ADZS-SC584-EZLITE EV-SC594-SOM + EV-SOMCCR-EZKIT
Version(s) 1.0.0-Github master (TBD) master (TBD)
Networking-1.0.0-Github telnet (TBD)

Feature Compatibility

Below are the feature compatibility matrices.

Audio Routing

Feature - Audio Codec IN/OUT USB RX/TX A2B RX/TX MIC IN SPDIF IN/OUT WAVE FILE IN/OUT VBAN RX/TX RTP RX/TX
Hardware Software Package
ADZS-SC589-MINI 1.0.0-Github YES YES YES NO YES YES NO NO
Networking-1.0.0-Github YES YES YES NO YES YES YES YES
ADZS-SC584-EZLITE master YES NO YES NO - To be implemented NO - To be implemented YES NO NO
telnet YES NO YES NO - To be implemented NO - To be implemented YES YES YES
EV-SC594-SOM + EV-SOMCCR-EZKIT master YES NO YES NO YES YES NO NO

Flash Storage

Feature - Storage SD Card WO (External Flash) SPIFFS (External Flash) MSD Host (USB Storage)
Hardware Software Package
ADZS-SC589-MINI 1.0.0-Github YES YES NO NO
Networking-1.0.0-Github YES YES NO NO
ADZS-SC584-EZLITE master NO NO YES NO
telnet NO NO YES NO
EV-SC594-SOM + EV-SOMCCR-EZKIT master NO YES YES NO

Communication

Feature - Communication UART over FTDI UART over USB/OTG Telnet Ethernet
Hardware Software Package
ADZS-SC589-MINI 1.0.0-Github NO YES NO NO
Networking-1.0.0-Github NO YES NO NO
ADZS-SC584-EZLITE master NO YES NO NO
telnet NO YES YES YES
EV-SC594-SOM + EV-SOMCCR-EZKIT master YES NO NO NO

Software Update

Feature - Software Update Update using CLPD via Bootswitch Update using SAM Flasher
Hardware Software Package
ADZS-SC589-MINI 1.0.0-Github NO YES
Networking-1.0.0-Github NO YES
ADZS-SC584-EZLITE master YES NO
telnet YES NO
EV-SC594-SOM + EV-SOMCCR-EZKIT master YES NO

Navigation - Advanced Audio Projects

resources/tools-software/sharc-audio-module/advanced-audio-projects/appendix-a.1684774876.txt.gz · Last modified: 22 May 2023 19:01 by Rebecca Butler