Wiki

This version is outdated by a newer approved version.DiffThis version (05 Feb 2021 00:55) was approved by Travis Collins.The Previously approved version (08 Jan 2021 23:23) is available.Diff

This is an old revision of the document!


ADI maintains a set of tools to model, interface, and target with ADI transceiver devices within MATLAB and Simulink. These are combined into a single Toolbox which contains a set of Board Support Packages (BSP). The list of supported boards is provided below.

Quick Start with Toolbox

The current stable Toolbox can be downloaded from the Sensor Toolbox GitHub Release Page. Download the latest mltbx file then open that file within MATLAB. Opening the file will automatically install the Toolbox, adding the necessary components to your MATLAB path. The “Analog Devices, Inc. Sensor Toolbox” will appear in your Add-Ons Explore within MATLAB.

To interface and stream data with hardware will require installation of libiio and one of two Hardware Support Packages from MathWorks. The libiio library can be obtained on the Github page of the project.

Libiio Installers

Installation of either:

is required to use the streaming system objects or blocks. These support packages provide the necessary libIIO MATLAB bindings used by ADI's system objects.

Builds for the master branches are available as well if you want to use something newer:

Master Branch (Pre-release) Installer

Toolbox Dependencies

Depending on your needs, different toolboxes will be required. For basic data streaming into MATLAB or Simulink only the following MathWorks toolboxes are required:

Device Control and Data Streaming

Device interfaces which provide control and data streaming are implemented with MATLAB System Objects and Simulink Blocks. These System Objects can be access under the “adi” namespace in MATLAB and are followed by their part number or board name:

adi.<Part or Board Name>

For example, to instantiate an ADIS16460 object to control IMU it can be created as follows:

imu = adi.ADIS16460;

For example usage of certain objects, it can be useful to inspect their related test code which exercises initiations in different configurations. The available code is available in the GitHub repo folder here, where object tests have the naming convention <Object>Tests.m.

To get a list of currently available objects with the BSP installed simply run:

help adi

To get more information on a given object run:

help adi.<Part of Board Name>

or

doc adi.<Part of Board Name>

Common Attributes

There are some common attributes that need to be set for system objects and parts.

  • uri Context address of IIO device. Possible options include:
    • IP with usage rx.uri = 'ip:192.168.2.1'
    • USB with usage rx.uri = 'usb:1.2.3'

Extending Interfaces

If a driver attribute or setting is not available in the standard objects it can be easily extended to cover more IIO attributes. See this guide.

Simulation Models of Hardware

Supported Boards

The following have device-specific implementations in MATLAB and Simulink. If a device has an IIO driver, MATLAB support is possible, but a device-specific MATLAB or Simulink interface may not exist yet.

Evaluation Card Streaming Support Targeting Variants and Minimum Supported Release
ADIS16375 Yes No ADI (R2019b)
ADIS16460 Yes No ADI (R2019b)
ADIS16480 Yes No ADI (R2019b)
ADIS16485 Yes No ADI (R2019b)
ADIS16488 Yes No ADI (R2019b)
CN0549 (CN0540+CN0532) Yes No ADI (R2020a)

Examples

Examples for streaming data are listed within the Toolbox documentation itself. To view run the following with MATLAB:

doc adi

Help & Support

resources/tools-software/sensor-toolbox.1612482912.txt.gz · Last modified: 05 Feb 2021 00:55 by Travis Collins