This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:product-support-software:sigma-delta_adc_temperature-ble_demo [03 Jan 2021 21:46] Robin Getz fix links |
resources:tools-software:product-support-software:sigma-delta_adc_temperature-ble_demo [14 Jan 2021 05:38] Robin Getz use wiki interwiki links |
||
---|---|---|---|
Line 2: | Line 2: | ||
===== Introduction ===== | ===== Introduction ===== | ||
- | This page gives an overview of using the Analog Devices Sigma Delta ADCs with Cortex-M3 ARM processor based [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EV-COG-AD3029.html#eb-overview | ADuCM3029 Cog Eval Board]]. The intended demo application shows how to convert an external sensor data into actual units and transmit them over either Bluetooth or UART link using ADIs [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EV-COG-AD3029.html#eb-overview | ADuCM3029 Cog board]] and [[https://wiki.analog.com/resources/eval/user-guides/ev-cog-bleintp1z | Bluetooth Eval board]]. The operation can be better illustrated using below diagram. | + | This page gives an overview of using the Analog Devices Sigma Delta ADCs with Cortex-M3 ARM processor based [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EV-COG-AD3029.html#eb-overview | ADuCM3029 Cog Eval Board]]. The intended demo application shows how to convert an external sensor data into actual units and transmit them over either Bluetooth or UART link using ADIs [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EV-COG-AD3029.html#eb-overview | ADuCM3029 Cog board]] and [[/resources/eval/user-guides/ev-cog-bleintp1z | Bluetooth Eval board]]. The operation can be better illustrated using below diagram. |
Line 55: | Line 55: | ||
=== 2) Interfacing ADuCM3029 Cog Board with Sigma Delta ADCs/Eval Board === | === 2) Interfacing ADuCM3029 Cog Board with Sigma Delta ADCs/Eval Board === | ||
- | The ADuCM3029 COG board is connected to Sigma Delta ADC Eval board using a [[https://wiki.analog.com/resources/eval/user-guides/ev-gear-expander1z | Gear Expander board]]. Depending upon the digital interface used on Sigma Delta ADCs, the connection could be either 4 line SPI or 3 line I2C. The connection can be done either using [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/sdp-breakout-board.html | SDP breakout board]] or by directly soldering fly wires from the ADC Evaluation board to ADuCM3029 Expander Gear board. The sample connection for the AD7124 Eval board with COG board is shown below using a fly wires. The wires are directly soldered on the Eval board, but for better connection, use the SDP breakout board: | + | The ADuCM3029 COG board is connected to Sigma Delta ADC Eval board using a [[/resources/eval/user-guides/ev-gear-expander1z | Gear Expander board]]. Depending upon the digital interface used on Sigma Delta ADCs, the connection could be either 4 line SPI or 3 line I2C. The connection can be done either using [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/sdp-breakout-board.html | SDP breakout board]] or by directly soldering fly wires from the ADC Evaluation board to ADuCM3029 Expander Gear board. The sample connection for the AD7124 Eval board with COG board is shown below using a fly wires. The wires are directly soldered on the Eval board, but for better connection, use the SDP breakout board: |
{{ :resources:tools-software:product-support-software:aducm3029-ad7124_eval.jpg?400 |}} | {{ :resources:tools-software:product-support-software:aducm3029-ad7124_eval.jpg?400 |}} | ||
Line 66: | Line 66: | ||
=== 3) Interfacing ADuCM3029 Cog Board with Bluetooth Eval Board === | === 3) Interfacing ADuCM3029 Cog Board with Bluetooth Eval Board === | ||
- | The below diagrams shows the connection between ADuCM3029 COG Board and Bluetooth Eval board. There are no additional jumper settings needed. Please refer [[https://wiki.analog.com/resources/eval/user-guides/ev-cog-bleintp1z | user manual]] for more details on the hardware connection: | + | The below diagrams shows the connection between ADuCM3029 COG Board and Bluetooth Eval board. There are no additional jumper settings needed. Please refer [[/resources/eval/user-guides/ev-cog-bleintp1z | user manual]] for more details on the hardware connection: |
== Primary-side == | == Primary-side == |