This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:product-support-software:ad717x_ad411x_mbed_example [03 Jan 2021 21:46] – fix links Robin Getz | resources:tools-software:product-support-software:ad717x_ad411x_mbed_example [15 May 2023 08:47] (current) – Added updated screenshot for the console menu Janani Sunil | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD717x/ | + | ====== AD717x/ |
===== Introduction ===== | ===== Introduction ===== | ||
Line 20: | Line 20: | ||
- | //*Note:The firmware provides a basic user-interface for interacting with the evaluation-board. All the main functionality of the AD411x/ | + | //*Note:The firmware provides a basic user-interface for interacting with the evaluation-board. All the main functionality of the AD411x/ |
- | This firmware can support the following members of the AD711x/ | + | |
+ | |||
+ | ====== Useful links====== | ||
+ | {{section> | ||
+ | * [[/ | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
Line 34: | Line 38: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | |||
- | ====== Useful links====== | ||
- | * [[https:// | ||
- | * [[https:// | ||
- | * [[https:// | ||
===== Hardware Connections ===== | ===== Hardware Connections ===== | ||
Line 57: | Line 56: | ||
===== AD717x Mbed Firmware ===== | ===== AD717x Mbed Firmware ===== | ||
- | ==== Downloads ==== | + | This section briefs on the usage of MBED firmware. This also explains the steps to compile and build the application |
+ | using mbed and //make// based build. | ||
<WRAP round download> | <WRAP round download> | ||
- | Latest | + | Source code is hosted here: |
- | * [[https:// | + | * [[repo> |
+ | |||
+ | Build Guide for Precision Converters MBED firmware (Use below link): | ||
+ | * [[:resources: | ||
</ | </ | ||
Line 80: | Line 83: | ||
* Start up a serial terminal emulator (e.g. Tera Term) | * Start up a serial terminal emulator (e.g. Tera Term) | ||
* Find the com-port your controller board is connected on and select it. | * Find the com-port your controller board is connected on and select it. | ||
- | * Set the baud-rate for 115200 | + | * Set the baud-rate for 230400 |
* Reset the controller board and connect. | * Reset the controller board and connect. | ||
* Use the menu provided over the terminal window to access the evaluation board. | * Use the menu provided over the terminal window to access the evaluation board. | ||
Line 88: | Line 91: | ||
The AD711x/ | The AD711x/ | ||
- | - Baud rate: 115200 | + | - Baud rate: 230400 |
- Data bits: 8-bits | - Data bits: 8-bits | ||
- Parity: None | - Parity: None | ||
Line 95: | Line 98: | ||
Configure your serial terminal ([[https:// | Configure your serial terminal ([[https:// | ||
- | {{ : | + | {{ : |
The AD717x/ | The AD717x/ | ||
- | {{ : | + | {{ : |
The firmware is designed to be intuitive to use, and requires little explanation, | The firmware is designed to be intuitive to use, and requires little explanation, |