This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:product-support-software:ad7124_temperature_measurement_demo [23 Jul 2021 12:42] – updated tera term settings Mahesh Phalke | resources:tools-software:product-support-software:ad7124_temperature_measurement_demo [20 Jul 2022 07:12] – updated keil studio section Mahesh Phalke | ||
---|---|---|---|
Line 17: | Line 17: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | * [[https://ide.mbed.com/compiler|Mbed Online Compiler]] | + | * [[https://studio.keil.arm.com/|Mbed Online Compiler]] |
* [[https:// | * [[https:// | ||
Line 47: | Line 47: | ||
=== Quick Start to use AD7124 Mbed Firmware === | === Quick Start to use AD7124 Mbed Firmware === | ||
- | If you have some familiarity with the Mbed platform, the following is a basic list of steps required to start running the code, see below for more detail: | + | If you have some familiarity with the Mbed platform, the following is a basic list of steps required to start running the code: |
* Connect the AD7124 EVAL-board to the SDP-K1 controller board as specified in hardware connections section. | * Connect the AD7124 EVAL-board to the SDP-K1 controller board as specified in hardware connections section. | ||
* Connect the SDP-K1 controller board to your computer over USB provided along with SDP-K1 board. | * Connect the SDP-K1 controller board to your computer over USB provided along with SDP-K1 board. | ||
- | * Go to the link of the code provided above in the ' | + | * Import |
- | * Ensure SDP-K1 controller board is selected (top right of online-compiler page). | + | {{ : |
- | * Compile the code. | + | |
- | * After a successful compile a binary will be downloaded to your computer | + | |
- | * Drag and drop this binary to the SDP-K1 USB drive mounted in your computer file system (similar to C/D drives). | + | |
- | {{ : | + | * Make sure all dependent libraries are obtained correctly by IDE. |
+ | {{ : | ||
+ | * Compile the code as shown below. After a successful compile a binary will be downloaded to your computer - store this into your computer. Drag and drop (or copy) this binary file to the SDP-K1 USB drive mounted in your computer file system (similar to C/D drives) to flash firmware into MCU. | ||
+ | {{ : | ||
---- | ---- |