This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:product-support-software:ad5592r_mbed_example [26 Apr 2021 17:42] – Updated EVB jumpers and hardware connections Michael Bradley | resources:tools-software:product-support-software:ad5592r_mbed_example [02 Aug 2021 08:52] – Pratyush Mallick | ||
---|---|---|---|
Line 91: | Line 91: | ||
* Start up a serial terminal emulator (e.g. Tera Term) | * Start up a serial terminal emulator (e.g. Tera Term) | ||
* Find the com-port your controller board is connected on and select it. | * Find the com-port your controller board is connected on and select it. | ||
- | * Set the baud-rate for 115200 | + | * Set the baud-rate for 230400 |
* Reset the controller board and connect. | * Reset the controller board and connect. | ||
* Use the menu provided over the terminal window to access the evaluation board. | * Use the menu provided over the terminal window to access the evaluation board. | ||
Line 104: | Line 104: | ||
The AD5592R/93R firmware example is configured to have following serial settings: | The AD5592R/93R firmware example is configured to have following serial settings: | ||
- | * Baud rate: 115200 | + | * Baud rate: 230400 |
* Data bits: 8-bits | * Data bits: 8-bits | ||
* Parity: None | * Parity: None | ||
Line 112: | Line 112: | ||
Configure your serial terminal ([[https:// | Configure your serial terminal ([[https:// | ||
- | {{ : | + | {{ : |
The AD5592R Main Menu looks like below (with Tera Term): | The AD5592R Main Menu looks like below (with Tera Term): |