This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:mathworks [16 Apr 2020 00:47] – [Device Data Streaming and Configuration] Travis Collins | resources:tools-software:mathworks [08 Jan 2021 23:23] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 3: | Line 3: | ||
{{ : | {{ : | ||
- | Analog Devices, Inc. (ADI) works directly with MathWorks to provide tools and interfaces to end-users to help in their evaluation, development, | + | Analog Devices, Inc. (ADI) works directly with MathWorks to provide tools and interfaces to end-users to help in their evaluation, development, |
===== Simulation Models ===== | ===== Simulation Models ===== | ||
Line 10: | Line 10: | ||
Simulation models of hardware devices are available from MathWorks directly or from ADI. These are behavioral models of specific parts, and should not be considered transistor-level simulation. The models are typically used to understand device configuration, | Simulation models of hardware devices are available from MathWorks directly or from ADI. These are behavioral models of specific parts, and should not be considered transistor-level simulation. The models are typically used to understand device configuration, | ||
- | * [[https:// | + | * [[adi>en/ |
- | * [[resources: | + | * [[resources: |
===== Device Data Streaming and Configuration ===== | ===== Device Data Streaming and Configuration ===== | ||
Line 17: | Line 17: | ||
{{ : | {{ : | ||
- | For users looking to configure a device and stream data directly back into MATLAB or Simulink, there are two main options available. Both rely on the [[https:// | + | For users looking to configure a device and stream data directly back into MATLAB or Simulink, there are two main options available. Both rely on the [[/ |
* FMComms 2/3/4/5 and ADRV9361 RFSOM: | * FMComms 2/3/4/5 and ADRV9361 RFSOM: | ||
* ADALM-PLUTO: | * ADALM-PLUTO: | ||
Line 25: | Line 25: | ||
* [[resources/ | * [[resources/ | ||
* [[resources/ | * [[resources/ | ||
- | Device-specific interfaces may not exist for all ADI products, but if a driver exists already adding support in MATLAB is a simple process. For a complete list of available drivers see [[https:// | + | * [[resources/ |
+ | Device-specific interfaces may not exist for all ADI products, but if a driver exists already adding support in MATLAB is a simple process. For a complete list of available drivers see [[/ | ||
===== Code Generation and Targeting ===== | ===== Code Generation and Targeting ===== | ||
Line 34: | Line 35: | ||
MathWorks offers direct HDL and C++ targeting support in the following Hardware Support Packages: | MathWorks offers direct HDL and C++ targeting support in the following Hardware Support Packages: | ||
- | * FMComms 2/3/4/5 and ADRV9361 RFSOM:[[https:// | + | * FMComms 2/3/4/5 and ADRV9361 RFSOM:[[mw>hardware-support/ |
- | * AD9361 based Ettus E310: [[https:// | + | * AD9361 based Ettus E310: [[mw>hardware-support/ |
As part of the relevant toolboxes, ADI provides support for varies different FPGA and ADI part combinations: | As part of the relevant toolboxes, ADI provides support for varies different FPGA and ADI part combinations: | ||
Line 44: | Line 45: | ||
===== Support ===== | ===== Support ===== | ||
- | Support for the toolboxes is provided online at EngineerZone under the [[https://ez.analog.com/ | + | Support for the toolboxes is provided online at EngineerZone under the [[ez>linux-device-drivers/ |