This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:mathworks [01 Aug 2019 17:23] – [Code Generation and Targeting] Travis Collins | resources:tools-software:mathworks [08 Jan 2021 23:23] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
===== MathWorks Support: MATLAB and Simulink Integrations ===== | ===== MathWorks Support: MATLAB and Simulink Integrations ===== | ||
- | Analog Devices Inc. (ADI) works directly with MathWorks to provide tools and interfaces to end-users to help in their evaluation, development, | + | {{ : |
+ | |||
+ | Analog Devices, Inc. (ADI) works directly with MathWorks to provide tools and interfaces to end-users to help in their evaluation, development, | ||
===== Simulation Models ===== | ===== Simulation Models ===== | ||
Line 8: | Line 10: | ||
Simulation models of hardware devices are available from MathWorks directly or from ADI. These are behavioral models of specific parts, and should not be considered transistor-level simulation. The models are typically used to understand device configuration, | Simulation models of hardware devices are available from MathWorks directly or from ADI. These are behavioral models of specific parts, and should not be considered transistor-level simulation. The models are typically used to understand device configuration, | ||
- | * [[https:// | + | * [[adi>en/ |
- | * [[resources: | + | * [[resources: |
===== Device Data Streaming and Configuration ===== | ===== Device Data Streaming and Configuration ===== | ||
Line 15: | Line 17: | ||
{{ : | {{ : | ||
- | For users looking to configure a device and stream data directly back into MATLAB or Simulink, there are two main options available. Both rely on the [[https:// | + | For users looking to configure a device and stream data directly back into MATLAB or Simulink, there are two main options available. Both rely on the [[/ |
- | * FMComms 2/3/4/5 and ADRV9361 RFSOM:[[https:// | + | * FMComms 2/3/4/5 and ADRV9361 RFSOM:[[mw>hardware-support/ |
- | * ADALM-PLUTO: | + | * ADALM-PLUTO: |
| | ||
If MathWorks does not support your current board or additional customization is required for a toolbox, ADI offers third-party open toolboxes which fills these gaps depending on your product category: | If MathWorks does not support your current board or additional customization is required for a toolbox, ADI offers third-party open toolboxes which fills these gaps depending on your product category: | ||
- | * Transceiver Toolbox | + | * [[resources/ |
- | * Sensor Toolbox | + | * [[resources/ |
- | * High-Speed Converter Toolbox | + | * [[resources/ |
- | * LIDAR Toolbox | + | * [[resources/ |
- | * Time-of-Flight Toolbox | + | Device-specific interfaces may not exist for all ADI products, but if a driver exists already adding support in MATLAB is a simple process. For a complete list of available drivers see [[/ |
- | + | ||
- | Device-specific interfaces may not exist for all ADI products, but if a driver exists already adding support in MATLAB is a simple process. For a complete list of available drivers see [[https:// | + | |
===== Code Generation and Targeting ===== | ===== Code Generation and Targeting ===== | ||
Line 35: | Line 35: | ||
MathWorks offers direct HDL and C++ targeting support in the following Hardware Support Packages: | MathWorks offers direct HDL and C++ targeting support in the following Hardware Support Packages: | ||
- | * FMComms 2/3/4/5 and ADRV9361 RFSOM:[[https:// | + | * FMComms 2/3/4/5 and ADRV9361 RFSOM:[[mw>hardware-support/ |
- | + | * AD9361 based Ettus E310: [[mw>hardware-support/ | |
- | As part of the relivant toolboxes ADI provides support for varies different FPGA and ADI part combinations: | + | |
- | * [[https:// | + | |
- | + | ||
- | https:// | + | |
- | https:// | + | |
- | ===== Configuration Tools ===== | + | As part of the relevant toolboxes, ADI provides support for varies different FPGA and ADI part combinations: |
+ | * [[resources/ | ||
+ | * [[resources/ | ||
===== Support ===== | ===== Support ===== | ||
+ | Support for the toolboxes is provided online at EngineerZone under the [[ez> |