This is an old revision of the document!
Analog Devices Inc. (ADI) works directly with MathWorks to provide tools and interfaces to end-users to help in their evaluation, development, and configuration of ADI hardware. This page outlines the different tools available for different products from ADI which can be used in different stages of a development cycle.
Simulation models of hardware devices are available from MathWorks directly or from ADI. These are behavioral models of specific parts, and should not be considered transistor-level simulation. The models are typically used to understand device configuration, digital signal path frequency responses, and non-idealities. Since they are pure simulation models they can be integrated with other channels models and receiver/transmitter algorithms. Models are available in the following places:
https://www.mathworks.com/discovery/sdr.html https://www.mathworks.com/hardware-support/adalm-pluto-radio.html https://www.mathworks.com/hardware-support/zynq-sdr.html
https://www.mathworks.com/discovery/sdr.html https://www.mathworks.com/hardware-support/zynq-sdr.html
The following have device-specific implementations in MATLAB and Simulink. If a device has an IIO driver, MATLAB support is possible, but a device-specific MATLAB or Simulink interface may not exist yet. If you would like one made please create a forum post on EngineerZone.
Evaluation Card | FPGA Board | Streaming Support | Targeting | Variants and Minimum Supported Release | Simulation Models |
---|---|---|---|---|---|
Pluto | Yes | Yes | ADI (2018b) MathWorks (2017a) | Yes | |
FMComms2/3/4 | Zedboard | Yes | Yes | ADI (2018b) MathWorks (2014b) | |
ZC702 | Yes | Yes | ADI (2018b) MathWorks (2014b) | ||
ZC706 | Yes | Yes | ADI (2018b) MathWorks (2014b) | ||
ZCU102 | Yes | Yes | ADI (2018b) MathWorks (2014b) | ||
ADRV9361-Z7035 | Yes | Yes | ADI (2018b) MathWorks (2015b) | ||
ADRV9364-Z7020 | Yes | Yes | ADI (2018b) | ||
ADRV9371/5 | ZC706 | Yes | Yes | ADI (2018b) | Yes |
ZCU102 | Yes | Yes | ADI (2018b) | ||
ZYNQ3 | Yes | No | ADI (2018b) | ||
ADRV9009/8 | ZC706 | Yes | No | ADI (2018b) | No |
ZCU102 | Yes | Yes | ADI (2018b) | ||
DAQ2 (AD9680/AD9144) | ZC706 | Yes | No | ADI (2018b) | No |
ZCU102 | Yes | No | ADI (2018b) | ||
AD9467 | Zedboard | Yes | No | ADI (2018b) | No |