This is an old revision of the document!
This release of Yocto Linux for ADSP-SC5xx Processors is a release specific to the ADSP-SC594 SOM board and ADSP-EZKIT Carrier board. This release does not support other ADSP-SC5xx processors that are supported by the 1.0 Release of Yocto Linux for ADSP-SC5xx Processors.
Once the other existing processors have been upgraded to the same versions of U-Boot, Linux and Yocto, this release will be merged and all processors will be supported under a single 2.0 release. At that point, support for this release will cease. All future maintenance for the ADSP-SC594 will then be incorporated into the main Yocto Linux Release.
The Yocto Linux for ADSP-SC5xx processors product is formally supported on Ubuntu 20.04 LTS 64-bit. While the product will likely build on other modern Linux distributions, ADI support for build issues will only be provided when using the supported Linux distribution.
The following processors and silicon revisions are supported by the Yocto Linux for ADSP-SC5xx product.
* ADSP-SC594 SOM-EZ in combination with the ADSP-EZKIT-CRR Carrier Board
The following system requirements are recommended:
For installation on the development board your host PC will require:
Note: The Yocto Linux product is built from source. For improved performance we recommend at least 4 cores and a SSD disk.
You can reach Analog Devices software and tools technical support in the following ways:
This is the first release of the Yocto Linux for ADSP-SC594 Processor. This is an intermediate release and it does not support any other processors. For existing supported processors please continue to use the 1.0 Release. The following changes have been applied since the 1.0 release of Yocto Linux for ADSP-SC5xx Processors.
HOME PAGE: Linux for ADSP-SC5xx Processors