This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:linuxdsp:releasenotes:rn-3.0.0 [12 May 2023 15:44] Vasileios Bimpikas Added glibc/musl disambiguation point |
resources:tools-software:linuxdsp:releasenotes:rn-3.0.0 [25 May 2023 11:44] Vasileios Bimpikas |
||
---|---|---|---|
Line 19: | Line 19: | ||
* ''adi_hybrid_audio'': Audio playback handled through SHARC firmware, codec control (volume, etc) is still available from Linux, ramdisk includes hybrid-audio package. This installs ''icap-device-example_Core1.ldr'' to ''/lib/firmware/adi_adsp_core1_fw.ldr'' | * ''adi_hybrid_audio'': Audio playback handled through SHARC firmware, codec control (volume, etc) is still available from Linux, ramdisk includes hybrid-audio package. This installs ''icap-device-example_Core1.ldr'' to ''/lib/firmware/adi_adsp_core1_fw.ldr'' | ||
- | * Added new ''adsp-sc5xx-tiny'' image (<16 MB) to enable ADSP-SC573 & ADSP-SC58* boards to be able to boot from SPI Flash | + | * Added new ''adsp-sc5xx-tiny'' image (<16 MB) to enable ADSP-SC573 & ADSP-SC58x boards to be able to boot from SPI Flash [[resources:tools-software:linuxdsp:docs:quickstartguide:boot-flash-sc58x-573|to enable ADSP-SC573 & ADSP-SC58* boards to be able to boot from SPI Flash]] |
* Added new boot methods: SD Card & USB Mass Storage for some of the supported boards: | * Added new boot methods: SD Card & USB Mass Storage for some of the supported boards: | ||
* SD Card Boot: | * SD Card Boot: | ||
Line 30: | Line 30: | ||
* ADSP-SC589-MINI | * ADSP-SC589-MINI | ||
* ADSP-SC589 EZ-KIT | * ADSP-SC589 EZ-KIT | ||
- | * To accommodate the smaller image footprint, the poky-tiny DISTRO is used instead of poky. The poky-tiny uses **''musl''** instead of **''glibc''** to reduce the overall image size. **''glibc''** can be re-instated following [[:resources:tools-software:linuxdsp:docs:quickstartguide:reinstate-glibc-3.0.0 | these steps]]. This will be turned into a distro option from the next release and on. | ||
* Added USB Audio Class 2.0 support and [[resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:device_mode:gadget_audio_3_0_0|example]] | * Added USB Audio Class 2.0 support and [[resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:device_mode:gadget_audio_3_0_0|example]] | ||
* Added Packet Engine Driver (PKTE) for ADSP-SC598 EZ-KIT. The supported algorithms are: ''adi-ecb-des3'', ''adi-ecb-des'', ''adi-ecb-aes'', ''adi-cbc-des3'', ''adi-cbc-des'', ''adi-cbc-aes'', ''adi-hmac-sha256'', ''adi-sha256'', ''adi-hmac-sha224'', ''adi-sha224'', ''adi-hmac-sha1'', ''adi-sha1'', ''adi-hmac-md5'' and ''adi-md5'' | * Added Packet Engine Driver (PKTE) for ADSP-SC598 EZ-KIT. The supported algorithms are: ''adi-ecb-des3'', ''adi-ecb-des'', ''adi-ecb-aes'', ''adi-cbc-des3'', ''adi-cbc-des'', ''adi-cbc-aes'', ''adi-hmac-sha256'', ''adi-sha256'', ''adi-hmac-sha224'', ''adi-sha224'', ''adi-hmac-sha1'', ''adi-sha1'', ''adi-hmac-md5'' and ''adi-md5'' |