This is an old revision of the document!
This release contains an upgrade of all the key components to a recent LTS release.
The Yocto Linux for ADSP-SC5xx processors product is formally supported on Ubuntu 20.04 LTS 64-bit. While the product will likely build on other modern Linux distributions, ADI support for build issues will only be provided when using the supported Linux distribution.
The following processors and silicon revisions are supported by the Yocto Linux for ADSP-SC5xx product.
Development Board | Supported Revision |
---|---|
ADSP-SC598 EZ-KIT | A or later |
ADSP-SC594 EZ-KIT | A or later |
ADSP-SC589 EZ-KIT | 2.0 or later |
ADSP-SC589-MINI | 1.5 or later |
ADSP-SC584 EZ-KIT | 2.0 or later |
ADSP-SC573 EZ-KIT | 2.0 or later |
The following system requirements are recommended:
For installation on the development board your host PC will require:
Note: The Yocto Linux product is built from source. For improved performance we recommend at least 4 cores and a SSD disk.
You can reach Analog Devices software and tools technical support in the following ways:
The following changes have been applied since the 1.0 release of Yocto Linux for ADSP-SC5xx Processors.
HOME PAGE: Linux for ADSP-SC5xx Processors