Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (03 Jul 2020 09:39) was approved by Sunny Feng.

This is an old revision of the document!


Setting Up The Sources

The following ADI managed repositories are used for the development of Linux for SC5xx:

URL Description Latest Development Branch Latest Release Branch
https://github.com/analogdevicesinc/lnxdsp-adi-meta ADI Yocto meta layer develop/yocto-1.0.0 N/A
https://github.com/analogdevicesinc/lnxdsp-repo-manifest Google repo manifest develop/yocto-1.0.0 N/A
https://github.com/analogdevicesinc/lnxdsp-scripts ADI scripts develop/yocto-1.0.0 N/A
https://github.com/analogdevicesinc/u-boot-sharc U-Boot Bootloader develop/yocto-1.0.0 N/A
https://github.com/analogdevicesinc/lnxdsp-linux Linux kernel develop/yocto-1.0.0 N/A

In order to simplify the checkout process, ADI recommends using Google's repo tool. To use the repo tool create a workspace directory and clone the tool:

mkdir <WORKSPACE>
cd <WORKSPACE>
mkdir bin
curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ./bin/repo
chmod a+x ./bin/repo

To set up the sources for development invoke repo with the path to the repo manifest and the active development branch:

./bin/repo init -u https://github.com/analogdevicesinc/lnxdsp-repo-manifest.git -b develop/yocto-1.0.0
./bin/repo sync

PREV: Setting Up The Host NEXT: Building The Components

resources/tools-software/linuxdsp/docs/quickstartguide/source-setup.1593761858.txt.gz · Last modified: 03 Jul 2020 09:37 by Sunny Feng