Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:linuxdsp:docs:quickstartguide:source-setup [03 Jul 2020 09:37] Sunny Fengresources:tools-software:linuxdsp:docs:quickstartguide:source-setup [24 Jul 2020 05:01] (current) Sunny Feng
Line 1: Line 1:
 ====== Setting Up The Sources ====== ====== Setting Up The Sources ======
 +
 +=== Repository URLs ===
 +
 The following ADI managed repositories are used for the development of Linux for SC5xx: The following ADI managed repositories are used for the development of Linux for SC5xx:
 +|<100% 46% 18% 18% 18%>|
 +^URL                                                       ^Description           ^Latest Development Branch   ^Latest Release Branch ^
 +|https://github.com/analogdevicesinc/lnxdsp-adi-meta       |ADI Yocto meta layer  |develop/yocto-1.0.0  |release/yocto-1.0.0  |
 +|https://github.com/analogdevicesinc/lnxdsp-repo-manifest  |Google repo manifest  |develop/yocto-1.0.0  |release/yocto-1.0.0  |
 +|https://github.com/analogdevicesinc/lnxdsp-scripts        |ADI scripts           |develop/yocto-1.0.0  |release/yocto-1.0.0  |
 +|https://github.com/analogdevicesinc/u-boot-sharc          |U-Boot Bootloader     |develop/yocto-1.0.0  |release/yocto-1.0.0  |
 +|https://github.com/analogdevicesinc/lnxdsp-linux          |Linux kernel          |develop/yocto-1.0.0  |release/yocto-1.0.0  |
 +|https://github.com/analogdevicesinc/lnxdsp-examples       |ADI SHARC examples    |develop/yocto-1.0.0  |release/yocto-1.0.0  |
  
-^URL                                                     ^ Description         ^ Latest Development Branch   ^ Latest Release Branch ^ +\\ 
-|https://github.com/analogdevicesinc/lnxdsp-adi-meta     | ADI Yocto meta layer|          develop/yocto-1.0.0|                  N/A | +=== Download Source code ===
-|https://github.com/analogdevicesinc/lnxdsp-repo-manifest| Google repo manifest|          develop/yocto-1.0.0|                  N/A | +
-|https://github.com/analogdevicesinc/lnxdsp-scripts      | ADI scripts                  develop/yocto-1.0.0|                  N/A | +
-|https://github.com/analogdevicesinc/u-boot-sharc        | U-Boot Bootloader            develop/yocto-1.0.0|     N/A | +
-|https://github.com/analogdevicesinc/lnxdsp-linux        | Linux kernel        |          develop/yocto-1.0.0|     N/A |+
  
 In order to simplify the checkout process, ADI recommends using Google's [[https://gerrit.googlesource.com/git-repo/|repo tool]]. To use the repo tool create a workspace directory and clone the tool: In order to simplify the checkout process, ADI recommends using Google's [[https://gerrit.googlesource.com/git-repo/|repo tool]]. To use the repo tool create a workspace directory and clone the tool:
Line 21: Line 28:
 To set up the sources for development invoke repo with the path to the repo manifest and the active development branch: To set up the sources for development invoke repo with the path to the repo manifest and the active development branch:
 <code> <code>
-./bin/repo init -u https://github.com/analogdevicesinc/lnxdsp-repo-manifest.git -b develop/yocto-1.0.0+./bin/repo init -u https://github.com/analogdevicesinc/lnxdsp-repo-manifest.git -b release/yocto-1.0.0
 ./bin/repo sync ./bin/repo sync
 </code> </code>
  
 +
 +After the sync finished, you would get files just like the picture shows below.
 +
 +{{:resources:tools-software:linuxdsp:docs:quickstartguide:yocto.png?400|}}
 +
 +\\
 +----
 **PREV:** [[resources/tools-software/linuxdsp/docs/quickstartguide/setting_up_your_host_pc|Setting Up The Host]] **NEXT:** [[resources/tools-software/linuxdsp/docs/quickstartguide/building|Building The Components]] **PREV:** [[resources/tools-software/linuxdsp/docs/quickstartguide/setting_up_your_host_pc|Setting Up The Host]] **NEXT:** [[resources/tools-software/linuxdsp/docs/quickstartguide/building|Building The Components]]
resources/tools-software/linuxdsp/docs/quickstartguide/source-setup.txt · Last modified: 24 Jul 2020 05:01 by Sunny Feng