Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:linuxdsp:docs:quickstartguide:quickstart_sc598_3_0_0 [24 May 2023 10:52]
Vasileios Bimpikas
resources:tools-software:linuxdsp:docs:quickstartguide:quickstart_sc598_3_0_0 [25 May 2023 10:33]
Vasileios Bimpikas
Line 133: Line 133:
 <code bash> <code bash>
 $ ls tmp/​deploy/​sdk $ ls tmp/​deploy/​sdk
-adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.host.manifest +adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.host.manifest 
-adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.sh +adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.sh 
-adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.target.manifest +adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.target.manifest 
-adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.testdata.json+adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.testdata.json
 </​code>​ </​code>​
  
-The ''​adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.sh''​ is a self-extracting archive containing the SDK.+The ''​adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.sh''​ is a self-extracting archive containing the SDK.
  
 === Installing the SDK === === Installing the SDK ===
 Invoke the self-extracting archive. Invoke the self-extracting archive.
-It will default to installing to ''/​opt/​adi-distro/​3.0.0''​ but gives you the option to select your own install folder during the installation.+It will default to installing to ''/​opt/​adi-distro-glibc/​3.0.0''​ but gives you the option to select your own install folder during the installation.
 For the minimal image on SC598 For the minimal image on SC598
 <code bash> <code bash>
-$ ./​adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.sh +$ ./​adi-distro-glibc-glibc-x86_64-adsp-sc5xx-minimal-cortexa55-adsp-sc598-som-ezkit-toolchain-3.0.0.sh 
-Analog Devices Inc Reference Distro SDK installer version 3.0.0 +Analog Devices Inc Reference Distro ​(glibc) ​SDK installer version 3.0.0 
-=============================================================== +======================================================================= 
-Enter target directory for SDK (default: /​opt/​adi-distro/​3.0.0):​ +Enter target directory for SDK (default: /​opt/​adi-distro-glibc/3.0.0): 
-Extracting SDK.........................................................................done+You are about to install the SDK to "/​opt/​adi-distro-glibc/​3.0.0"​. Proceed [Y/n]? 
 +Extracting SDK....................................................................................................................done
 Setting it up...done Setting it up...done
 SDK has been successfully set up and is ready to be used. SDK has been successfully set up and is ready to be used.
 Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
- $ . /​opt/​adi-distro/​3.0.0/​environment-setup-cortexa55-adi-linux-musl+ $ . /​opt/​adi-distro-glibc/​3.0.0/​environment-setup-cortexa55-adi_glibc-linux
 </​code>​ </​code>​
  
Line 199: Line 200:
   ;''​**Terminal2:​ OpenOCD**''​   ;''​**Terminal2:​ OpenOCD**''​
   :<code bash>   :<code bash>
-$ sdk_usr=/​opt/​adi-distro/​3.0.0/​sysroots/​x86_64-adisdk-linux/usr/+$ sdk_usr=/​opt/​adi-distro-glibc/​3.0.0/​sysroots/​x86_64-adi_glibc_sdk-linux/usr/
 $ $sdk_usr/​bin/​openocd -f $sdk_usr/​share/​openocd/​scripts/​interface/<​ICE>​.cfg -f $sdk_usr/​share/​openocd/​scripts/​target/​adspsc59x_a55.cfg $ $sdk_usr/​bin/​openocd -f $sdk_usr/​share/​openocd/​scripts/​interface/<​ICE>​.cfg -f $sdk_usr/​share/​openocd/​scripts/​target/​adspsc59x_a55.cfg
 </​code>​ </​code>​
Line 227: Line 228:
   : <code bash>   : <code bash>
 $ cd /tftpboot $ cd /tftpboot
-$ /​opt/​adi-distro/​3.0.0/​sysroots/​x86_64-adisdk-linux/​usr/​bin/​aarch64-adi-linux/​aarch64-adi-linux-gdb u-boot-spl-sc598-som-ezkit.elf+$ /​opt/​adi-distro-glibc/​3.0.0/​sysroots/​x86_64-adi_glibc_sdk-linux/​usr/​bin/​aarch64-adi_glibc-linux/​aarch64-adi_glibc-linux-gdb u-boot-spl-sc598-som-ezkit.elf
 ... ...
 (gdb) target extended-remote :3333 (gdb) target extended-remote :3333
resources/tools-software/linuxdsp/docs/quickstartguide/quickstart_sc598_3_0_0.txt · Last modified: 25 May 2023 10:33 by Vasileios Bimpikas