This is an old revision of the document!
The build system is currently supported on host PCs running Ubuntu 20.04 LTS 64-bit.
In order to build and deploy Linux to your ADSP-SC598-EZKIT development board you will need to install the following packages on your host PC.
$ sudo apt-get update $ sudo apt-get install -y gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev xterm u-boot-tools openssl curl tftpd-hpa python
CrossCore Embedded Studio contains OpenOCD which is used to transfer U-Boot into RAM for the first initial boot of the device. The tools are created for 32-bit architecture and therefore requires a 32-bit libz package to run. Download and install it.
$ wget https://download.analog.com/tools/CrossCoreEmbeddedStudio/Releases/Release_2.11.0/adi-CrossCoreEmbeddedStudio-linux-x86-2.11.0.deb $ sudo dpkg -i ./adi-CrossCoreEmbeddedStudio-linux-x86-2.11.0.deb $ sudo apt install lib32z1
A TFTP server on the host is used to transfer images to the development board. Install and configure.
$ sudo vi /etc/default/tftpd-hpa #Replace the existing file with the following TFTP_USERNAME="tftp" TFTP_DIRECTORY="/tftpboot" TFTP_ADDRESS="0.0.0.0:69" TFTP_OPTIONS="--secure" #End of File $ sudo mkdir /tftpboot $ sudo chmod 777 /tftpboot $ sudo service tftpd-hpa restart
In order to communicate with the U-Boot bootloader, a UART connection must be made between the host PC and the development board. It is recommended that you use minicom to do this. Minicom must be configured to connect to U-Boot correctly.
On the host PC open a terminal and execute the following commands:
$ sudo apt-get install -y minicom $ sudo minicom -s +-----[configuration]------+ | Filenames and paths | | File transfer protocols | | Serial port setup | | Modem and dialing | | Screen and keyboard | | Save setup as dfl | | Save setup as.. | | Exit | | Exit from Minicom | +--------------------------+ # Select Serial port setup Set Serial Device to /dev/ttyUSB0 Set Bps/Par/Bits to 115200 8N1 Set Hardware Flow Control to No Close the Serial port setup option by press Esc Select Save setup as dfl Select Exit
The example is fully contained in the Analog Devices Yocto Linux github repositories.
To install the sources: TODO: Make sure its the correct repo, branch, manifest file etc
$ mkdir ~/gxp2 $ cd ~/gxp2 $ mkdir bin $ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ./bin/repo $ chmod a+x ./bin/repo $ ./bin/repo init \ -u https://github.com/analogdevicesinc/lnxdsp-repo-manifest.git \ -b develop/yocto-2.2.0 \ -m develop-yocto-2.2.0.xml $ ./bin/repo sync
Yocto requires the environment to be configured before building is possible. A setup-environment script in the gxp2 folder contains all the required environment settings for your build target. Source the setup script for your board:
$ source setup-environment -m adsp-sc598-som-ezkit
Sourcing the script will configure your build environment and create a build folder along with a local build configuration file. See the Yocto Manual for further details.
You can build three different versions of the root filesystem; minimal, ramdisk and full. To build the example images invoke bitbake from within the build directory created previously.
$ bitbake adsp-sc5xx-minimal $ bitbake adsp-sc5xx-ramdisk $ bitbake adsp-sc5xx-full
When the build completes you will see a warning that the ELF binary has relocations in .text. It is OK to ignore this warning
Copy the U-Boot Proper elf files to the tftp directory:
$ cp tmp/deploy/images/adsp-sc598-som-ezkit/u-boot-proper-sc598-som-ezkit.elf /tftpboot/
Before installing the software on to the development board, ensure that the following cables are connected:
The console output from U-Boot and later on Linux will appear on the USB serial port configured in minicom earlier so open up minicom.
Terminal1: minicom
$ sudo minicom
In a separate console launch OpenOCD and connect to the development board.
Terminal2: OpenOCD
$ cd /opt/analog/cces/2.11.0/ARM/openocd/share/openocd/scripts $ sudo /opt/analog/cces/2.11.0/ARM/openocd/bin/openocd -f interface/<ICE>.cfg -f board/ev-sc598-som.cfg
Where <ICE>
should be replaced with ice1000
or ice2000
depending on your hardware.
When successful you should see a message similar to the console output below
Open On-Chip Debugger (Analog Devices CCES 2.11.0) OpenOCD 0.10.0-gd1ba667 (2022-04-13-15:58) Licensed under GNU GPL v2 Report bugs to <processor.tools.support@analog.com> Info : only one transport option; autoselect 'jtag' adapter speed: 5000 kHz Info : halt and restart using CTI adspsc59x_a55_init Info : Listening on port 6666 for tcl connections Info : Listening on port 4444 for telnet connections Info : ICE-1000 firmware version is 1.0.2 Info : clock speed 5000 kHz Info : JTAG tap: adspsc598.adjc tap/device found: 0x0282e0cb (mfg: 0x065 (Analog Devices), part: 0x282e, ver: 0x0) Info : JTAG tap: adspsc598.cpu enabled Info : DAP adspsc598.cpu DPIDR indicates ADIv6 protocol is being used Info : adspsc598.cpu: hardware has 6 breakpoints, 4 watchpoints Info : starting gdb server for adspsc598.cpu on 3333 Info : Listening on port 3333 for gdb connections
In a third console window launch GDB and type target extended-remote :3333
. This will make GDB to connect to the gdbserver on the local host using port 3333. Then, load the U-Boot into RAM by typing load u-boot-proper-sc598-som-ezkit.elf
.
Terminal3: GDB
$ cd /tftpboot $ /opt/analog/cces/2.11.0/ARM/aarch64-none-elf/bin/aarch64-none-elf-gdb u-boot-proper-sc598-som-ezkit.elf ... (gdb) target extended-remote :3333 Remote debugging using :3333 0x000000000000352c in ?? () (gdb) load u-boot-proper-sc598-som-ezkit.elf Loading section .text, size 0x150 lma 0x96000000 Loading section .efi_runtime, size 0xfb0 lma 0x96000150 Loading section .text_rest, size 0x5ad94 lma 0x96001800 Loading section .rodata, size 0x12f1c lma 0x9605c598 Loading section .hash, size 0x18 lma 0x9606f4b8 Loading section .dtb.init.rodata, size 0xac0 lma 0x9606f4d0 Loading section .data, size 0x47e8 lma 0x9606ff90 Loading section .got, size 0x8 lma 0x96074778 Loading section .got.plt, size 0x18 lma 0x96074780 Loading section .u_boot_list, size 0x2800 lma 0x96074798 Loading section .efi_runtime_rel, size 0x1b0 lma 0x96076f98 Loading section .rela.dyn, size 0xb700 lma 0x96077148 Start address 0x96000000, load size 532800 Transfer rate: 29 KB/sec, 12685 bytes/write. (gdb) c Continuing.
At this point U-Boot will now be running in RAM on your target board. You should see U-Boot booting in the minicom console (Terminal 1). Press a key to interrupt the boot process before the countdown terminates:
Terminal1: minicom
U-Boot 2020.10 (Aug 23 2022 - 13:09:23 +0000) Model: ADI sc598-som-ezkit Watchdog enabled I2C: ready DRAM: 224 MiB MMC: mmc@310C7000: 0 Loading Environment from SPIFlash... SF: Detected is25lp512 with page size 256 Bytes, erase size 64 KiB, total 64 MiB OK In: serial@0x31003000 Out: serial@0x31003000 Err: serial@0x31003000 Net: eth0: eth@0x31040000 Hit any key to stop autoboot: 0 =>
The U-Boot console is used to copy U-Boot (SPL and Proper), the minimal root filesystem image and the fitImage (which contains the kernel image and dtb file) into RAM and then write them to Flash. Copy the required files from <BUILD DIR>/tmp/deploy/images to your /tftpboot directory.
$ cp tmp/deploy/images/adsp-sc598-som-ezkit/stage1-boot.ldr /tftpboot/ $ cp tmp/deploy/images/adsp-sc598-som-ezkit/stage2-boot.ldr /tftpboot/ $ cp tmp/deploy/images/adsp-sc598-som-ezkit/fitImage /tftpboot/ $ cp tmp/deploy/images/adsp-sc598-som-ezkit/adsp-sc5xx-minimal-adsp-sc598-som-ezkit.jffs2 /tftpboot
In the U-Boot console, set the IP address of the Host Linux PC that hosts the binary files on TFTP. Also, set the same address to the variable serverip
Terminal1: minicom
=> setenv tftpserverip <SERVERIP> => setenv serverip <SERVERIP>
ip addr
command from the shell or console.
If your network supports DHCP, run:
=> run update_qspi_sc598
If your network does NOT support DHCP, in the U-Boot console configure the board IP address and remove the “run init_ethernet;” from the “update_spi_sc598” command.
=> setenv ipaddr <IPADDR> => edit update_spi_sc598 => edit: <remove "run init_ethernet;" from here> sf probe ${sfdev}; sf erase 0 ${sfsize}; run update_spi_uboot; run update_spi_fit; run update_spi_rfs; sleep 3; saveenv => run update_qspi_sc598
After removing “run init_ethernet;” from update_spi_sc598, issue the “run update_qspi_sc598” command as above.
You should see output similar to the following.
=> run update_qspi_sc598 PHY 0x00: OUI = 0x80028, Model = 0x23, Rev = 0x01, 100baseT, FDX SF: Detected is25lp512 with page size 256 Bytes, erase size 64 KiB, total 64 MiB SF: 67108864 bytes @ 0x0 Erased: OK Speed: 1000, full duplex Using eth@0x31040000 device TFTP from server 10.37.33.116; our IP address is 10.37.33.113 Filename 'stage1-boot.ldr'. Load address: 0x96000000 Loading: ###### 3.6 MiB/s done Bytes transferred = 79480 (13678 hex) SF: Detected is25lp512 with page size 256 Bytes, erase size 64 KiB, total 64 MiB device 0 offset 0x0, size 0x13678 SF: 79480 bytes @ 0x0 Written: OK Speed: 1000, full duplex Using eth@0x31040000 device TFTP from server 10.37.33.116; our IP address is 10.37.33.113 Filename 'stage2-boot.ldr'. Load address: 0x96000000 Loading: ######################################### 5.2 MiB/s done Bytes transferred = 592288 (909a0 hex) SF: Detected is25lp512 with page size 256 Bytes, erase size 64 KiB, total 64 MiB device 0 offset 0x20000, size 0x909a0 SF: 592288 bytes @ 0x20000 Written: OK Speed: 1000, full duplex Using eth@0x31040000 device TFTP from server 10.37.33.116; our IP address is 10.37.33.113 Filename 'fitImage'. Load address: 0x96000000 Loading: ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ###################################################### 5.6 MiB/s done Bytes transferred = 14149218 (d7e662 hex) SF: Detected is25lp512 with page size 256 Bytes, erase size 64 KiB, total 64 MiB device 0 offset 0x160000, size 0xd7e662 SF: 14149218 bytes @ 0x160000 Written: OK Speed: 1000, full duplex Using eth@0x31040000 device TFTP from server 10.37.33.116; our IP address is 10.37.33.113 Filename 'adsp-sc5xx-minimal-adsp-sc598-som-ezkit.jffs2'. Load address: 0x96000000 Loading: ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ############################## 5.6 MiB/s done Bytes transferred = 30015488 (1ca0000 hex) SF: Detected is25lp512 with page size 256 Bytes, erase size 64 KiB, total 64 MiB device 0 offset 0x1000000, size 0x1ca0000 SF: 30015488 bytes @ 0x1000000 Written: OK Saving Environment to SPIFlash... Erasing SPI flash...Writing to SPI flash...done OK =>
The U-Boot image, root filesystem and Linux kernel are now stored in QSPI. Adjust the BOOT MODE selector to position 1 and press the RESET button, the board should boot into Linux.
... [ OK ] Started Login Service. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@ @@@@@@@@ @@@@@@@ @@@@@@@@ @@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ Analog Devices Yocto Distribution www.analog.com www.yoctoproject.org adsp-sc598-som-ezkit login: root Password: adi root@adsp-sc598-som-ezkit:~#
The username is root and the password is adi.
In order to boot Linux, the TFTP server should be setup as above and (for both NFS and RAM boot) a copy of the kernel image and dtb file should be copied into the /tftpboot directory.
$ cp tmp/deploy/images/adsp-sc598-som-ezkit/Image /tftpboot $ cp tmp/deploy/images/adsp-sc598-som-ezkit/sc598-som-ezkit.dtb /tftpboot
For RAM boot a copy of the image containing the filesystem needs copied to the /tftpboot directory.
$ cp tmp/deploy/images/adsp-sc598-som-ezkit/adsp-sc5xx-ramdisk-adsp-sc598-som-ezkit.cpio.xz.u-boot /tftpboot/ramdisk.cpio.xz.u-boot
For NFS boot we use the Network File System which is stored in local Ubuntu Host. This is suggested when you do application development. To setup the NFS server:
$ sudo apt-get install nfs-kernel-server $ sudo vi /etc/exports #Add following commands /romfs *(rw,sync,no_root_squash,no_subtree_check) $ sudo mkdir /romfs/ $ sudo chmod 777 /romfs/ $ sudo service nfs-kernel-server start
The root filesystem should then be copied to /romfs.
$ sudo tar -xf tmp/deploy/images/adsp-sc598-som-ezkit/adsp-sc5xx-full-adsp-sc598-som-ezkit.tar.xz -C /romfs
Next, on the target, from u-boot, run one of the following command:
=> run ramboot or => run nfsboot ...... ...... Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@ @@@@@@@@ @@@@@@@ @@@@@@@@ @@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ Analog Devices Yocto Distribution www.analog.com www.yoctoproject.org adsp-sc598-som-ezkit login: root Password: adi root@adsp-sc598-som-ezkit:~#
To build the SDK follow the instructions here Building the SDK.