This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linuxdsp:docs:quickstartguide:quickstart_sc594 [28 Sep 2022 10:21] – Removed SHARC-ALSA example instructions Henrik Mau | resources:tools-software:linuxdsp:docs:quickstartguide:quickstart_sc594 [24 Nov 2022 14:32] – Vasileios Bimpikas | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== Yocto Linux Quickstart Guide for ADSP-SC594 ===== | + | ===== Yocto Linux 2.1.0 Quickstart Guide for ADSP-SC594 ===== |
- | <note important> | + | <note important> |
===== Setting Up Your Host PC ===== | ===== Setting Up Your Host PC ===== | ||
Line 199: | Line 199: | ||
: < | : < | ||
$ cd /tftpboot | $ cd /tftpboot | ||
- | $ / | + | $ / |
... | ... | ||
(gdb) target extended-remote :3333 | (gdb) target extended-remote :3333 | ||
Remote debugging using :3333 | Remote debugging using :3333 | ||
0x000000000000352c in ?? () | 0x000000000000352c in ?? () | ||
- | (gdb) load u-boot-spl-sc594-som-ezkit.elf | ||
- | Loading section .text, size 0x13618 lma 0x20080000 | ||
- | Start address 0x20080000, load size 79384 | ||
- | Transfer rate: 34 KB/sec, 15876 bytes/ | ||
- | (gdb) c | ||
- | Continuing. | ||
- | ^C | ||
- | Program received signal SIGINT, Interrupt. | ||
- | 0x0000000020080ca0 in ?? () | ||
- | </ | ||
- | |||
- | At this point you should see the following message in the first terminal. | ||
- | |||
- | ;'' | ||
- | : | ||
- | < | ||
- | U-Boot SPL 2020.10 (Aug 23 2022 - 13:09:23 +0000) | ||
- | ADI Boot Mode: 0 (JTAG/ | ||
- | SPL execution has completed. | ||
- | </ | ||
- | |||
- | Back in the third terminal, load U-Boot Proper into RAM. | ||
- | |||
- | ;'' | ||
- | : | ||
- | < | ||
(gdb) load | (gdb) load | ||
Loading section .text, size 0x150 lma 0x96000000 | Loading section .text, size 0x150 lma 0x96000000 |