Wiki

This version is outdated by a newer approved version.DiffThis version (24 May 2023 10:55) was approved by Vasileios Bimpikas.The Previously approved version (24 May 2023 10:53) is available.Diff

This is an old revision of the document!


Yocto Linux 3.0.0 Quickstart Guide for ADSP-SC589 (EZKIT & MINI)

The following instructions are for the ADSP-SC589-EZKIT and ADSP-SC589-MINI development boards. For instructions for other processors and development boards please refer to Linux for ADSP-SC5xx Processors 3.0.0

Setting Up Your Host PC

The build system is currently supported on host PCs running Ubuntu 20.04 LTS 64-bit.


Installing Required Packages

In order to build and deploy Linux to your ADSP-SC589-EZKIT or ADSP-SC589-MINI development board you will need to install the following packages on your host PC.

$ sudo apt-get update
$ sudo apt-get install -y gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev xterm u-boot-tools openssl curl tftpd-hpa python3 zstd liblz4-tool

Configuring TFTP Service

A TFTP server on the host is used to transfer images to the development board. Install and configure.

$ sudo vi /etc/default/tftpd-hpa
 
#Replace the existing file with the following
TFTP_USERNAME="tftp"
TFTP_DIRECTORY="/tftpboot"
TFTP_ADDRESS="0.0.0.0:69"
TFTP_OPTIONS="--secure"
#End of File
 
$ sudo mkdir /tftpboot
$ sudo chmod 777 /tftpboot
$ sudo service tftpd-hpa restart


Configure Minicom

In order to communicate with the U-Boot bootloader, a UART connection must be made between the host PC and the development board. It is recommended that you use minicom to do this. Minicom must be configured to connect to U-Boot correctly.

On the host PC open a terminal and execute the following commands:

$ sudo apt-get install -y minicom
$ sudo minicom -s
 
            +-----[configuration]------+
            | Filenames and paths      |
            | File transfer protocols  |
            | Serial port setup        |
            | Modem and dialing        |
            | Screen and keyboard      |
            | Save setup as dfl        |
            | Save setup as..          |
            | Exit                     |
            | Exit from Minicom        |
            +--------------------------+
 
 
# Select Serial port setup
     Set Serial Device to /dev/ttyUSB0
     Set Bps/Par/Bits to 115200 8N1
     Set Hardware Flow Control to No
 
     Close the Serial port setup option by press Esc
 Select Save setup as dfl
 Select Exit
/dev/ttyUSB0 might not correspond to the serial port of the board on every system. You can determine which /dev entry your board uses by running ls -l /dev/ttyUSB* twice, once when the serial port of the board is plugged in, and once when it isn't.


Installing the Sources

The example is fully contained in the Analog Devices Yocto Linux github repositories.

To install the sources: 

$ mkdir ~/griffin
$ cd ~/griffin
$ mkdir bin
$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ./bin/repo
$ chmod a+x ./bin/repo
$ ./bin/repo init \
   -u https://github.com/analogdevicesinc/lnxdsp-repo-manifest.git \
   -b release/yocto-3.0.0 \
   -m release-yocto-3.0.0.xml
$ ./bin/repo sync


Building the Image

Preparing the buildtool

Yocto requires the environment to be configured before building is possible.  A setup-environment script in the griffin folder contains all the required environment settings for your build target. Source the setup script for your board:

$ source setup-environment -m adsp-sc589-ezkit

or

$ source setup-environment -m adsp-sc589-mini

Sourcing the script will configure your build environment and create a build folder along with a local build configuration file.  See the Yocto Manual for further details.

Note that the build environment needs to be sourced once only before building.  If later working in a different terminal the setup-environment script should be sourced again.  If sourcing the setup-environment script is done without specifying the machine Yocto will reuse the previous configuration settings and retain any changes made to the files in the conf folder.


Building the example

You can build three different versions of the root file system; tiny, minimal and full. To build the example images invoke bitbake from within the build directory created previously.

$ bitbake adsp-sc5xx-tiny
$ bitbake adsp-sc5xx-minimal
$ bitbake adsp-sc5xx-full

When the build completes you will see a warning that the ELF binary has relocations in .text. It is OK to ignore this warning

Building a Linux distribution with Yocto is a significantly demanding process, both in CPU and network usage. A full build from scratch is estimated to take around 170 minutes for an 11th Gen Intel Core i5-11500T with 16 GB of RAM and a stable, fast Internet connection. This estimate can go up significantly for a poorer Internet connection or CPU resources, so set aside plenty of time for a clean build.

Building the SDK

The SDK will provide you with the cross toolchain needed to develop application for the target board, alongside various miscellaneous tools. Notably, it will provide you with OpenOCD and GDB, which you can use to run and flash U-Boot on the board.

The SDK can be built for the adsp-sc5xx-minimal image or the adsp-sc5xx-full image. To build the SDK for the adsp-sc5xx-minimal image invoke bitbake from within the build directory created previously.

$ bitbake adsp-sc5xx-minimal -c populate_sdk

or for the adsp-sc5xx-full image

$ bitbake adsp-sc5xx-full -c populate_sdk

When the build has completed you will find a set of files in the <BUILD_DIR>/tmp/deploy/sdk directory. For example, the minimal image on SC589-EZKIT:

$ ls tmp/deploy/sdk
adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc589-ezkit-toolchain-3.0.0.host.manifest
adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc589-ezkit-toolchain-3.0.0.sh
adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc589-ezkit-toolchain-3.0.0.target.manifest
adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc589-ezkit-toolchain-3.0.0.testdata.json

The adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc589-ezkit-toolchain-3.0.0.sh or adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc589-mini-toolchain-3.0.0.sh is a self-extracting archive containing the SDK.

Installing the SDK

Invoke the self-extracting archive. It will default to installing to /opt/adi-distro/3.0.0 but gives you the option to select your own install folder during the installation. For the minimal image on SC589-EZKIT

$ ./adi-distro-musl-x86_64-adsp-sc5xx-minimal-cortexa5t2hf-neon-adsp-sc589-ezkit-toolchain-3.0.0.sh
Analog Devices Inc Reference Distro SDK installer version 3.0.0
===============================================================
Enter target directory for SDK (default: /opt/adi-distro/3.0.0):
You are about to install the SDK to "/opt/adi-distro/3.0.0". Proceed [Y/n]? y
Extracting SDK........................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
 $ . /opt/adi-distro/3.0.0/environment-setup-cortexa5t2hf-neon-adi-linux-musleabi

Your SDK is now installed.

Running U-Boot on the Board for the first time

It's always good practice to erase the contents of /tftpboot/ before running and/or flashing a new build of U-Boot or Linux. You can do so by executing rm /tftpboot/* before proceeding

Copy the U-Boot binary & loader files to the tftp directory:

$ cp tmp/deploy/images/adsp-sc589-ezkit/u-boot-proper-sc589-ezkit.elf /tftpboot
$ cp tmp/deploy/images/adsp-sc589-ezkit/u-boot-spl-sc589-ezkit.elf /tftpboot
$ cp tmp/deploy/images/adsp-sc589-ezkit/stage1-boot.ldr /tftpboot
$ cp tmp/deploy/images/adsp-sc589-ezkit/stage2-boot.ldr /tftpboot

or

$ cp tmp/deploy/images/adsp-sc589-mini/u-boot-proper-sc589-mini.elf /tftpboot
$ cp tmp/deploy/images/adsp-sc589-mini/u-boot-spl-sc589-mini.elf /tftpboot
$ cp tmp/deploy/images/adsp-sc589-mini/stage1-boot.ldr /tftpboot
$ cp tmp/deploy/images/adsp-sc589-mini/stage2-boot.ldr /tftpboot

Before installing the software on to the development board, ensure that the following cables are connected:

  • Board connected to network via ethernet cable using J14 connector.
  • Board connected to host PC using USB micro cable, connected to USB/UART port on the development board
  • Board connected to the ICE 1000 or ICE 2000 via the DEBUG port on the board
  • ICE is also connected to host PC via USB mini cable

  • ADSP-SC589-EZKIT only: The BOOT MODE selector on the board should be turned to “0”.

The console output from U-Boot and later on Linux will appear on the USB serial port configured in minicom earlier so open up minicom.

Terminal1: minicom
$ sudo minicom 

In a separate console launch OpenOCD and connect to the development board

Terminal2: OpenOCD
$ sdk_usr=/opt/adi-distro/3.0.0/sysroots/x86_64-adisdk-linux/usr/
$ $sdk_usr/bin/openocd -f $sdk_usr/share/openocd/scripts/interface/<ICE>.cfg -f $sdk_usr/share/openocd/scripts/board/adspsc589_ezbrd.cfg

Where <ICE> should be replaced with ice1000 or ice2000 depending on your hardware. When successful you should see a message similar to the console output below

    Open On-Chip Debugger (PKGVERSION)  OpenOCD 0.10.0-g40378454d (2023-04-05-10:35)
    Licensed under GNU GPL v2 
    Report bugs to <processor.tools.support@analog.com>
    adapter speed: 1000 kHz 
    Info : transports supported by the debug adapter: "jtag", "swd"
    Info : auto-select transport "jtag"
    halt and restart using CTI
    trst_only separate trst_push_pull
    Info : ICE-1000 firmware version is 1.0.2
    Info : clock speed 1000 kHz
    Info : JTAG tap: adspsc58x.adjc tap/device found: 0x228080cb (mfg: 0x065, part: 0x2808, ver: 0x2)
    Info : JTAG tap: adspsc58x.dap enabled
    Info : adspsc58x.dap: hardware has 3 breakpoints, 2 watchpoints
    Info : adspsc58x.dap: but you can only set 1 watchpoint

In a third console window launch GDB and type target extended-remote :3333. This will make GDB to connect to the gdbserver on the local host using port 3333. Then, load the spl file into RAM by typing load and run it by typing c. Hit Ctrl+C to interrupt thereafter.

Terminal3: GDB (sc589-ezkit)
$ cd /tftpboot
$ /opt/adi-distro/3.0.0/sysroots/x86_64-adisdk-linux/usr/bin/arm-adi-linux-gnueabi/arm-adi-linux-gnueabi-gdb u-boot-spl-sc589-ezkit.elf
...
Reading symbols from u-boot-spl-sc589-ezkit.elf...done.
(gdb) target extended-remote :3333
Remote debugging using :3333
0x00004884 in ?? ()
(gdb) load
Loading section .text, size 0x9f2c lma 0x20080000
Loading section .rodata, size 0x1198 lma 0x20089f2c
Loading section .dtb.init.rodata, size 0x12c0 lma 0x2008b0d0
Loading section .data, size 0x514 lma 0x2008c390
Loading section .u_boot_list, size 0xa50 lma 0x2008c8a4
Start address 0x20080000, load size 53992
Transfer rate: 30 KB/sec, 7713 bytes/write.
(gdb) c
Continuing.
^C
Program received signal SIGINT, Interrupt.
Terminal3: GDB (sc589-mini)
$ cd /tftpboot
$ /opt/adi-distro/3.0.0/sysroots/x86_64-adisdk-linux/usr/bin/arm-adi-linux-gnueabi/arm-adi-linux-gnueabi-gdb u-boot-spl-sc589-mini.elf
...
Reading symbols from u-boot-spl-sc589-mini.elf...done.
(gdb) target extended-remote :3333
Remote debugging using :3333
0x00004884 in ?? ()
(gdb) load
Loading section .text, size 0x9f2c lma 0x20080000
Loading section .rodata, size 0x1198 lma 0x20089f2c
Loading section .dtb.init.rodata, size 0x12c0 lma 0x2008b0d0
Loading section .data, size 0x514 lma 0x2008c390
Loading section .u_boot_list, size 0xa50 lma 0x2008c8a4
Start address 0x20080000, load size 53992
Transfer rate: 30 KB/sec, 7713 bytes/write.
(gdb) c
Continuing.
^C
Program received signal SIGINT, Interrupt.

You will see a message on Terminal 1 running minicom, informing you that you can now load U-Boot Proper

Terminal1: minicom
U-Boot SPL 2020.10 (Mar 16 2023 - 13:07:24 +0000)
ADI Boot Mode: 0x0 (JTAG/BOOTROM)
SPL execution has completed.  Please load U-Boot Proper via JTAG

Now, load U-Boot Proper into RAM.

Terminal3: GDB (sc589-ezkit)
(gdb) load u-boot-proper-sc589-ezkit.elf
Loading section .text, size 0x3a8 lma 0xc2200000
Loading section .text_rest, size 0x48bd8 lma 0xc22003c0
Loading section .rodata, size 0x1037d lma 0xc2248f98
Loading section .hash, size 0x18 lma 0xc2259318
Loading section .dtb.init.rodata, size 0x17f0 lma 0xc2259330
Loading section .data, size 0x2410 lma 0xc225ab20
Loading section .got.plt, size 0xc lma 0xc225cf30
Loading section .u_boot_list, size 0x170c lma 0xc225cf3c
Loading section .rel.dyn, size 0xa3b0 lma 0xc225e648
Loading section .dynsym, size 0x30 lma 0xc22689f8
Loading section .dynstr, size 0x1 lma 0xc2268a28
Loading section .dynamic, size 0x90 lma 0xc2268a2c
Loading section .gnu.hash, size 0x18 lma 0xc2268abc
Start address 0xc2200000, load size 428726
Transfer rate: 31 KB/sec, 11587 bytes/write.
(gdb) c
Continuing.
Terminal3: GDB (sc589-mini)
(gdb) load u-boot-proper-sc589-mini.elf
Loading section .text, size 0x3a8 lma 0xc2200000
Loading section .text_rest, size 0x48bd8 lma 0xc22003c0
Loading section .rodata, size 0x1037d lma 0xc2248f98
Loading section .hash, size 0x18 lma 0xc2259318
Loading section .dtb.init.rodata, size 0x17f0 lma 0xc2259330
Loading section .data, size 0x2410 lma 0xc225ab20
Loading section .got.plt, size 0xc lma 0xc225cf30
Loading section .u_boot_list, size 0x170c lma 0xc225cf3c
Loading section .rel.dyn, size 0xa3b0 lma 0xc225e648
Loading section .dynsym, size 0x30 lma 0xc22689f8
Loading section .dynstr, size 0x1 lma 0xc2268a28
Loading section .dynamic, size 0x90 lma 0xc2268a2c
Loading section .gnu.hash, size 0x18 lma 0xc2268abc
Start address 0xc2200000, load size 428726
Transfer rate: 31 KB/sec, 11587 bytes/write.
(gdb) c
Continuing.

At this point U-Boot will now be running in RAM on your target board. You should see U-Boot booting in the minicom console (Terminal 1). Press a key to interrupt the boot process before the countdown terminates:

Terminal1: minicom (sc589-ezkit)
U-Boot 2020.10 (Mar 16 2023 - 13:07:24 +0000)
 
CPU:   ADSP ADSP-SC589-0.1 (spi flash boot)
Detected Revision: 1.1
Model: ADI sc589-ezkit
DRAM:  224 MiB
WDT:   Not found!
MMC:   mmc0@31010000: 0
Loading Environment from SPIFlash... SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB
OK
In:    serial@0x31003000
Out:   serial@0x31003000
Err:   serial@0x31003000
Net:   eth0: eth0
Hit any key to stop autoboot:  0
=>
Terminal1: minicom (sc589-mini)
U-Boot 2020.10 (Mar 16 2023 - 13:07:24 +0000)
 
CPU:   ADSP ADSP-SC589-0.1 (spi flash boot)
Detected Revision: 1.1
Model: ADI sc589-mini
DRAM:  224 MiB
WDT:   Not found!
MMC:   mmc0@31010000: 0
Loading Environment from SPIFlash... SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB
OK
In:    serial@0x31003000
Out:   serial@0x31003000
Err:   serial@0x31003000
Net:   eth0: eth0
Hit any key to stop autoboot:  0
=>


Flash U-Boot to SPI Flash


In the U-Boot console, set the IP address of the Linux PC that hosts the U-Boot loader files (stage1-boot.ldr & stage2-boot.ldr) on TFTP.

Terminal1: minicom
=> setenv serverip <SERVERIP>
=> setenv tftpserverip <SERVERIP>
To find the IP address of your host Linux PC you can issue the ip addr command from the shell or console.

If your network supports DHCP, run:

=> dhcp

If your network does NOT support DHCP, run:

=> set ipaddr <ADDR>

Where <ADDR> is the IP address you want to assign.

If flashing a board that had been previously programmed, it's good to erase the whole flash before as sometimes previous U-Boot installations might leave remnants. You can do that by typing ⇒ sf probe ${sfdev}; sf erase 0 0x4000000 on the U-Boot prompt before proceeding to the following instructions

Next, run the U-Boot update command to copy the U-Boot loader files from the host PC to the target board, and write it into flash:

=> run update_spi_uboot_only

You will see an output similar to the one below:

=> run update_spi_uboot_only
Speed: 1000, full duplex
Using eth0 device
TFTP from server 192.168.1.223; our IP address is 192.168.1.217
Filename 'stage1-boot.ldr'.
Load address: 0xc2000000
Loading: ####
         2.5 MiB/s
done
Bytes transferred = 54068 (d334 hex)
SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB
device 0 offset 0x0, size 0xd334
SF: 54068 bytes @ 0x0 Written: OK
Speed: 1000, full duplex
Using eth0 device
TFTP from server 192.168.1.223; our IP address is 192.168.1.217
Filename 'stage2-boot.ldr'.
Load address: 0xc2000000
Loading: ##############################
         3.4 MiB/s
done
Bytes transferred = 429012 (68bd4 hex)
SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB
device 0 offset 0x20000, size 0x68bd4
SF: 429012 bytes @ 0x20000 Written: OK

In order to store the serverip and the DHCP or otherwise assigned IP address of the board and have them available on next boot, you can run the following command:

=> saveenv
Saving Environment to SPIFlash... Erasing SPI flash...Writing to SPI flash...done
OK

At this point the U-Boot binary is stored in flash. You can now disconnect the ICE-1000 or ICE-2000 from the development board and make sure to switch the BMODE to position 1. You will only need to reconnect this if your board fails to boot and you need to re-follow these instructions.

Booting Linux

Booting Linux from SPI Flash

The ADSP-SC589-EZKIT and ADSP-SC589-MINI come equipped with 16 MiB of SPI Flash. The adsp-sc5xx-tiny image can be stored into it and used to boot Linux from it. You can do this from the U-Boot prompt. Following the guide so far, you'll have U-Boot installed into SPI Flash and getting the U-Boot prompt when powering up the board with the boot selector set to '1'.

You'd first need to copy the fitImage and the tiny root filesystem on the TFTP server directory of the Host machine:

$ cp tmp/deploy/images/adsp-sc589-ezkit/fitImage /tftpboot/
$ cp tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-tiny-adsp-sc589-ezkit.jffs2 /tftpboot/

or

$ cp tmp/deploy/images/adsp-sc589-mini/fitImage /tftpboot/
$ cp tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-tiny-adsp-sc589-mini.jffs2 /tftpboot/

In order to flash the kernel on the flash, run the below command and observe a similar output:

=> run update_spi_fit
Speed: 1000, full duplex
Using eth0 device
TFTP from server 192.168.1.223; our IP address is 192.168.1.217
Filename 'fitImage'.
Load address: 0xc2000000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ################################
         3.6 MiB/s
done
Bytes transferred = 6193382 (5e80e6 hex)
SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB
device 0 offset 0xe0000, size 0x5e80e6
SF: 6193382 bytes @ 0xe0000 Written: OK

Now run the following command to also flash the root filesystem:

=> run update_spi_rfs
Speed: 1000, full duplex
Using eth0 device
TFTP from server 192.168.1.223; our IP address is 192.168.1.217
Filename 'adsp-sc5xx-tiny-adsp-sc589-ezkit.jffs2'.
Load address: 0xc2000000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ##
         3.6 MiB/s
done
Bytes transferred = 9568256 (920000 hex)
SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB
device 0 offset 0x6e0000, size 0x920000
SF: 9568256 bytes @ 0x6e0000 Written: OK

You are now ready to boot into Linux, by entering run spiboot on the U-Boot prompt:

=> run spiboot
SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB
device 0 offset 0xe0000, size 0x5e80e6
SF: 6193382 bytes @ 0xe0000 Read: OK
## Loading kernel from FIT Image at c2000000 ...
   Using 'conf-1' configuration
   Verifying Hash Integrity ... OK
   Trying 'kernel-1' kernel subimage
     Description:  Linux kernel
     Type:         Kernel Image
     Compression:  uncompressed
     Data Start:   0xc20000dc
     Data Size:    4774696 Bytes = 4.6 MiB
     Architecture: ARM
     OS:           Linux
     Load Address: 0x80008000
     Entry Point:  0x80008000
     Hash algo:    sha1
     Hash value:   24bf0dc6adfde94b1e336f0ab5623bf5ec8d9c1e
     Sign algo:    sha1,rsa2048:
     Sign value:   unavailable
   Verifying Hash Integrity ... sha1+ sha1,rsa2048:- OK
 
...
 
systemd-journald[153]: Oldest entry in /run/log/journal/0e090b939c924da8bc4494744ba9ea15/system.journal is older than the configured file retention duration (1month), suggesting rotation.
systemd-journald[153]: /run/log/journal/0e090b939c924da8bc4494744ba9ea15/system.journal: Journal header limits reached or header out-of-date, rotating.
 
 
     @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@  @@@@@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@     @@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@        @@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@            @@@@@@@@@@@@@@@@@@@
     @@@@@@@@               @@@@@@@@@@@@@@@@
     @@@@@@@@                   @@@@@@@@@@@@
     @@@@@@@@                     @@@@@@@@@@
     @@@@@@@@                        @@@@@@@
     @@@@@@@@                     @@@@@@@@@@
     @@@@@@@@                   @@@@@@@@@@@@
     @@@@@@@@               @@@@@@@@@@@@@@@@
     @@@@@@@@            @@@@@@@@@@@@@@@@@@@
     @@@@@@@@        @@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@     @@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@  @@@@@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
 
        Analog Devices Yocto Distribution
                 www.analog.com
              www.yoctoproject.org
 
adsp-sc589-ezkit login: root
Password: adi

Booting Linux Using SD Card

Formatting the SD Card

In order to use an SD Card with Linux we need to prepare it by formatting it in the correct format. This section of instructions requires you to correctly identify the SD Card and format the card. If you select the wrong drive you may cause irreversible damage to you Host PC. To format the SD Card, follow the commands below. The example code in this section assumes that the SD Card device is reported to be /dev/sdb. Ensure that you change these commands to use your device.

$ sudo fdisk /dev/sdb
/* Create primary partition 1, 256M size*/
Command (m for help): n
Select (default p): p
Partition number (1-4, default 1): 1
First sector (2048-3887103, default 2048): PRESS ENTER
Last sector, +sectors or +size{K,M,G} (2048-3887103, default 3887103): PRESS ENTER
 
/* Save partition */
Command (m for help): w

Format the SD card to EXT filesystem

$ sudo mkfs.ext2 /dev/sdb1


Writing the kernel and file system to the SD Card

Next, we need to copy the Linux file system and kernel image to the SD Card. We install this on to the SD Card by mounting the file system on to the local Host PC and copying the contents on to the SD Card. To allow the choice of booting using ramboot and sdcard boot we copy the ramboot image to the SD card as well as extract the minimal image to the SD card.

$ mkdir ~/mnt
$ sudo mount -t ext2 /dev/sdb1 ~/mnt
$ sudo mkdir ~/mnt/boot
$ sudo cp tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-ramdisk-adsp-sc589-ezkit.cpio.xz ~/mnt/boot/ramdisk.cpio.xz.u-boot
$ sudo cp tmp/deploy/images/adsp-sc589-ezkit/sc589-ezkit.dtb ~/mnt/boot/
$ sudo cp tmp/deploy/images/adsp-sc589-ezkit/fitImage ~/mnt/boot/
$ sudo tar -xf tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-minimal-adsp-sc589-ezkit.tar.xz -C ~/mnt
$ sudo umount ~/mnt

or

$ mkdir ~/mnt
$ sudo mount -t ext2 /dev/sdb1 ~/mnt
$ sudo mkdir ~/mnt/boot
$ sudo cp tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-ramdisk-adsp-sc589-mini.cpio.xz ~/mnt/boot/ramdisk.cpio.xz.u-boot
$ sudo cp tmp/deploy/images/adsp-sc589-mini/sc589-mini.dtb ~/mnt/boot/
$ sudo cp tmp/deploy/images/adsp-sc589-mini/fitImage ~/mnt/boot/
$ sudo tar -xf tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-minimal-adsp-sc589-mini.tar.xz -C ~/mnt
$ sudo umount ~/mnt

The file system and kernel image are now installed on to the SD Card. The SD Card can now be safely removed from the Host PC.


Booting Linux from the SD card

Insert the SD card to target board, and reset the board and enter into U-Boot

=> run sdcardboot
or 
=> run ramboot_emmc

The linux kernel will then boot up using the file system stored in SD card.


Booting Linux from USB Mass Storage

Formating USB stick

Frist step is to format USB stick to U-Boot supported formats.

To format the USB stick, follow the commands below. The example code in this section assumes that the USB device is reported to be /dev/sdb. Ensure that you change these commands to use your device.

$ sudo fdisk /dev/sdb
/* Create primary partition 1, 256M size*/
Command (m for help): n
Select (default p): p
Partition number (1-4, default 1): 1
First sector (2048-3887103, default 2048): PRESS ENTER
Last sector, +sectors or +size{K,M,G} (2048-3887103, default 3887103): PRESS ENTER
 
/* Save partition */
Command (m for help): w

Format the USB stick to EXT4 filesystem

$ sudo mkfs.ext4 /dev/sdb1

Writing kernel and rootfs image to USB stick

$ mkdir ~/mnt
$ sudo mount -t ext4 /dev/sdb1 ~/mnt
$ sudo mkdir ~/mnt/boot
$ sudo cp tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-ramdisk-adsp-sc589-ezkit.cpio.xz ~/mnt/boot/ramdisk.cpio.xz.u-boot
$ sudo cp tmp/deploy/images/adsp-sc589-ezkit/fitImage ~/mnt/boot/
$ sudo umount ~/mnt

or for SC598-mini

$ mkdir ~/mnt
$ sudo mount -t ext4 /dev/sdb1 ~/mnt
$ sudo mkdir ~/mnt/boot
$ sudo cp tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-ramdisk-adsp-sc589-mini.cpio.xz ~/mnt/boot/ramdisk.cpio.xz.u-boot
$ sudo cp tmp/deploy/images/adsp-sc589-mini/fitImage ~/mnt/boot/
$ sudo umount ~/mnt

Booting Linux from USB Mass Storage

To boot from ADSP-SC589-EZKIT run this commands in u-boot

setenv usbload 'ext4load usb 0 ${initramaddr} /boot/${initramfile}; ext4load usb 0 ${loadaddr} /boot/${imagefile};'
setenv usbboot 'usb start; run usbload; run ramargs; bootm ${loadaddr} ${initramaddr};'
run usbboot

To boot from ADSP-SC589-MINI there is need to disable emac0 device in u-boot device tree, as USB and ethernet port share same pin and can't run simultaneously. Inside Yocto directory type

devtool modify u-boot-adi

edit build/workspace/sources/u-boot-adi/arch/arm/dts/sc589-mini.dts by adding

&emac0 {
    status="disable";
};

To rebuild U-boot after modifications

devtool build u-boot-adi

Booting rootfs from USB Mass Storage

Follow the step how to setup USB stick in chapter above. Set environment variables in U-boot

setenv usbargs 'setenv bootargs root=/dev/sda1 rw rootfstype=ext4 rootwait earlycon=adi_uart,0x31003000 console=ttySC0,115200'
setenv usbload 'ext4load usb 0 ${loadaddr} /boot/${imagefile};'
setenv usbboot 'usb start; run usbload; run usbargs; bootm ${loadaddr};'

And type to boot

run usbboot

Now the rootfs is set to your USB stick and amount of space equals of size of partition on USB stick.


Booting Linux Using TFTP

In order to boot Linux, the TFTP server should be setup as above and a copy of the kernel image should be copied into the /tftpboot directory.

$ cp tmp/deploy/images/adsp-sc589-ezkit/fitImage /tftpboot

or

$ cp tmp/deploy/images/adsp-sc589-mini/fitImage /tftpboot


NFS Boot

For NFS boot we use the Network File System which is stored in local Ubuntu Host. This is suggested when you do application development. To setup the NFS server:

$ sudo apt-get install nfs-kernel-server
$ sudo vi /etc/exports
 
#Add following commands
/romfs *(rw,sync,no_root_squash,no_subtree_check)
 
$ sudo mkdir /romfs/
$ sudo chmod 777 /romfs/
$ sudo service nfs-kernel-server start

We can verify that the NFS service is running by executing

$ sudo service nfs-kernel-server status

The output will indicate that the server is active, i.e.

● nfs-server.service - NFS server and services
     Loaded: loaded (/lib/systemd/system/nfs-server.service; enabled; vendor preset: enabled)
    Drop-In: /run/systemd/generator/nfs-server.service.d
             └─order-with-mounts.conf
     Active: active (exited) since Tue 2022-09-06 14:38:31 BST; 3 months 14 days ago
   Main PID: 953 (code=exited, status=0/SUCCESS)
      Tasks: 0 (limit: 18797)gxp2
     Memory: 0B
     CGroup: /system.slice/nfs-server.service
 
Sep 06 14:38:29 $YOUR_HOSTNAME systemd[1]: Starting NFS server and services...
Sep 06 14:38:31 $YOUR_HOSTNAME systemd[1]: Finished NFS server and services.

If it's reported as inactive, wait a few moments and check the status again.

The root filesystem should then be copied to /romfs.

If you are using the ADSP-SC589-EZKIT with the full image (you ran 'bitbake adsp-sc5xx-full'):

$ sudo tar -xf tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-full-adsp-sc589-ezkit.tar.xz -C /romfs

Or if you are using the ADSP-SC589-EZKIT with the minimal image (you ran 'bitbake adsp-sc5xx-minimal'):

$ sudo tar -xf tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-minimal-adsp-sc589-ezkit.tar.xz -C /romfs

Or if you are using the ADSP-SC589-MINI with the full image (you ran 'bitbake adsp-sc5xx-full'):

$ sudo tar -xf tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-full-adsp-sc589-mini.tar.xz -C /romfs

Or if you are using the ADSP-SC589-MINI with the minimal image (you ran 'bitbake adsp-sc5xx-minimal'):

$ sudo tar -xf tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-minimal-adsp-sc589-mini.tar.xz -C /romfs


Booting into Linux from TFTP

Next, on the target, from u-boot, run the following command:

=> run nfsboot
......
......
         Starting Update UTMP about System Runlevel Changes...
[  OK  ] Started Update UTMP about System Runlevel Changes.
 
 
     @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@  @@@@@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@     @@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@        @@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@            @@@@@@@@@@@@@@@@@@@
     @@@@@@@@               @@@@@@@@@@@@@@@@
     @@@@@@@@                   @@@@@@@@@@@@
     @@@@@@@@                     @@@@@@@@@@
     @@@@@@@@                        @@@@@@@
     @@@@@@@@                     @@@@@@@@@@
     @@@@@@@@                   @@@@@@@@@@@@
     @@@@@@@@               @@@@@@@@@@@@@@@@
     @@@@@@@@            @@@@@@@@@@@@@@@@@@@
     @@@@@@@@        @@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@     @@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@  @@@@@@@@@@@@@@@@@@@@@@@@@@@@@
     @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
 
        Analog Devices Yocto Distribution
                 www.analog.com
              www.yoctoproject.org
 
adsp-sc589-ezkit login: root
Password: adi
root@adsp-sc589-ezkit:~#

The default username is root and the password is adi.

resources/tools-software/linuxdsp/docs/quickstartguide/quickstart_sc589_3_0_0.1684918511.txt.gz · Last modified: 24 May 2023 10:55 by Vasileios Bimpikas